Power Management Fundamentals II Session 4: Isolated Converters Explained

    What does isolation mean for power topologies? Let's review what galvanic isolation means and go through the terminology and standards. We'll explore isolation...
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
    • Maximize Your Power Regulator: Key Considerations for Thermal Performance
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC's Quizzes AQQ296 about repairing an equation in a digital display

      1. Quote of this month: " When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Too Much Chatter and Not Enough Talk - Learn the Benefits...
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
    The Power Problem Inside Every AI Breakthrough: Part 1 of 3

    Artificial intelligence isn’t just changing how we interact with the world; it’s transforming the very hardware that makes it all possible. As AI invades...

     

    Simplifying Stability with EVAL-KW4503Z: Part 1 of 3

    Sensors are all around us. They help our gadgets, appliances, and electronic equipment "notice" what's happening in our environment. Essentially, they...

    Latest Blogs

    • Energy Transfer Considerations in Isolated SMPS: Part 2 of 4
    • Automating LTspice .NOISE Measurements with .STEP and .MEAS Directives: Part 2 of 3
    • ​​Channel Specification: The Key to GMSL Compliance​
    • Understanding Voltage Domain Isolation in Field-Bus Systems
    • Ethernet-APL’s Impact on Functional, Intrinsic, and Cyber Safety
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
SigmaDSP Processors & SigmaStudio Dev. Tool
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
SigmaDSP Processors & SigmaStudio Dev. Tool
  • Processors & DSP
SigmaDSP Processors & SigmaStudio Dev. Tool
Documents Implementing Safeload Writes on the ADAU1701
  • Q&A
  • File Uploads
  • Members
  • Tags
  • Cancel
  • Documents
  • SigmaDSP YouTube Channel - Dave Thib
  • +AD193x: FAQ
  • +ADAU1401AEBZ: FAQ
  • +ADAU144x: FAQ
  • +ADAU1452: FAQ
  • +ADAU145x: FAQ
  • -ADAU1701: FAQ
    • ADAU1701 Input and Output Signal Routing
    • ADAU1701: ADC resistor values for higher sample rates
    • Implementing Safeload Writes on the ADAU1701
    • My 2IN4OUT Proto with SPDIF based on ADAU1701
    • Setting the PLL mode for the ADAU1701 at different sample rates
    • Thoughts on using index selectable filters...
    • Using hardware data capture (trap) registers with the DSP Readback cell (AD1940, ADAU1701)
  • +ADAU1701MINIZ- FAQ
  • +ADAU1761: FAQ
  • +ADAU1772: FAQ
  • +ADI: FAQ
  • +AN-951: FAQ
  • +bitwise logic: FAQ
  • +Compressor Table Format: FAQ
  • +Creating a simple balance crossfade control: FAQ
  • +Creating constant-dB envelope decay using an existing linear decay algorithm: FAQ
  • +Crossover with more than 3 bands: FAQ
  • +E2PROM: FAQ
  • +EEPROM: FAQ
  • +EVAL DAU144XEBZ: FAQ
  • +EVAL-ADAU1781Z: FAQ
  • +Excluding Cells from the Exported System Files: FAQ
  • +GPIO button: FAQ
  • +GPIOs or Aux ADCs: FAQ
  • +How do I execute a software safeload write?: FAQ
  • +IIR coefficient filter: FAQ
  • +IIR filter: FAQ
  • +Peak Full Range Compressor: FAQ
  • +Preserving "Ear-candy": FAQ
  • +Push Button Volume: FAQ
  • +self-boot EEPROM image: FAQ
  • +Sigma300 Family Products: FAQ
  • +SigmaDSP: FAQ
  • +SigmaStudio: FAQ
  • +single precision VS double precision: FAQ
  • +Stimulus-Probe Capability and Limitations: FAQ
  • +Stopwatch to Count Successive Samples: FAQ
  • +Toolbox into the schematic tab: FAQ
  • +USB communications between the PC and SigmaDSP: FAQ
  • +Using Hierarchy Boards to create re-usable code: FAQ
  • New SigmaStudio 3.2.0 beta version available
  • SigmaStudio 3.3 Released
  • SigmaStudio 3.9.2 Beta Available for Download
  • SigmaStudio Rev 3.15.2 Bug Report for SPI EEPROM Write Speed

Implementing Safeload Writes on the ADAU1701

In order to use the safeload write feature on the ADAU1701 (also ADAU1702, ADAU1401, and ADAU1401A), a very specific sequence of write commands must be executed. The write sequence is as follows:

  • Safeload Data 0, address 0x0810
  • Safeload Address 0, address 0x0815
  • (optional) Safeload Data 1, address 0x0811
  • (optional) Safeload Address 1, address 0x0816
  • (optional) Safeload Data 2, address 0x0812
  • (optional) Safeload Address 2, address 0x0817
  • (optional) Safeload Data 3, address 0x0813
  • (optional) Safeload Address 3, address 0x0818
  • (optional) Safeload Data 4, address 0x0814
  • (optional) Safeload Address 4, address 0x0819
  • Initiate safeload transfer bit, address 0x081C

Up to 5 target addresses may be written. The writes marked "optional" in the list above only need to be included if more than one parameter is being updated.

The format for the Safeload Address and Safeload Data registers is as follows (from the ADAU1701 datasheet):

A simple example of using the Safeload Data 0, Safeload Address 0, and IST (initiate safeload transfer bit) to set a volume control to 0 dB in parameter memory is shown below. In this example, the target address in parameter RAM is 0x0000. Since only one parameter is being updated, the Data 1, Data 2, Data 3, Data 4, Address 1, Address 2, Address 3, and Address 4 registers may be ignored.

//Write 0x00800000 to set volume to 0 dB

08 10 00 00 80 00 00     //Data 0
08 15 00 00              //Address 0
08 1C 00 3C              //Set IST High

In the case where multiple parameters need to be updated, the additional parameter data and address registers may be used. The following example shows the 5 parameters of an IIR filter being updated.

//Write 1kHz, +5 dB peaking filter coefficients

08 10 00 00 83 57 7E     //Data 0
08 15 00 00              //Address 0
08 11 00 FF 0A B4 47     //Data 1
08 16 00 01              //Address 1
08 12 00 00 74 12 18     //Data 2
08 17 00 02              //Address 2
08 13 00 00 F5 4B B9     //Data 3
08 18 00 03              //Address 3
08 14 00 FF 88 96 6B     //Data 4
08 19 00 04              //Address 4
08 1C 00 3C              //Set IST High

Only one safeload write operation should be attempted per each audio frame.

Tags: adau1702 adau1401 safeload_write safeload adau1701
  • Share
  • History
  • More
  • Cancel
 
Related Content
  • How do I execute a software safeload write?
    Sara Collins
    In order to use software safeload to write data to parameter RAM, at least three writes must be performed. First, the data is loaded into the safeload data registers (addresses 0x0001 through 0x0005),...
  • Software safeload examples
    ADIApproved
    In order to use software safeload to write data to parameter RAM, at least three writes must be performed. First, the data is loaded into the safeload data registers (addresses 0x0001 through 0x0005),...
  • ADAU1467 SPI Microcontroller Safeload Tutorial
    mike177
    Hello, I hope that this post is helpful, I did not find documentation for SPI Safeload Write using a microcontroller on ADAU1467 so I will share my discoveries. 1. (Not shown in the waveform) toggle...
 
Related Content
  • How do I execute a software safeload write?
    Sara Collins
    In order to use software safeload to write data to parameter RAM, at least three writes must be performed. First, the data is loaded into the safeload data registers (addresses 0x0001 through 0x0005),...
  • Software safeload examples
    ADIApproved
    In order to use software safeload to write data to parameter RAM, at least three writes must be performed. First, the data is loaded into the safeload data registers (addresses 0x0001 through 0x0005),...
  • ADAU1467 SPI Microcontroller Safeload Tutorial
    mike177
    Hello, I hope that this post is helpful, I did not find documentation for SPI Safeload Write using a microcontroller on ADAU1467 so I will share my discoveries. 1. (Not shown in the waveform) toggle...