Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp Open Loop Gain and LTspice

      A kind proposal from Al Butvidas 1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

EngineerZone
EngineerZone
SigmaDSP Processors & SigmaStudio Dev. Tool
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
SigmaDSP Processors & SigmaStudio Dev. Tool
  • Processors & DSP
SigmaDSP Processors & SigmaStudio Dev. Tool
Documents Can I program multiple SigmaDSPs in parallel using one USBi?
  • Q&A
  • File Uploads
  • Members
  • Tags
  • Cancel
  • Documents
  • SigmaDSP YouTube Channel - Dave Thib
  • +AD193x: FAQ
  • +ADAU1401AEBZ: FAQ
  • +ADAU144x: FAQ
  • +ADAU1452: FAQ
  • +ADAU145x: FAQ
  • +ADAU1701: FAQ
  • +ADAU1701MINIZ- FAQ
  • +ADAU1761: FAQ
  • +ADAU1772: FAQ
  • +ADI: FAQ
  • +AN-951: FAQ
  • +bitwise logic: FAQ
  • +Compressor Table Format: FAQ
  • +Creating a simple balance crossfade control: FAQ
  • +Creating constant-dB envelope decay using an existing linear decay algorithm: FAQ
  • +Crossover with more than 3 bands: FAQ
  • +E2PROM: FAQ
  • +EEPROM: FAQ
  • +EVAL DAU144XEBZ: FAQ
  • +EVAL-ADAU1781Z: FAQ
  • +Excluding Cells from the Exported System Files: FAQ
  • +GPIO button: FAQ
  • +GPIOs or Aux ADCs: FAQ
  • +How do I execute a software safeload write?: FAQ
  • +IIR coefficient filter: FAQ
  • +IIR filter: FAQ
  • +Peak Full Range Compressor: FAQ
  • +Preserving "Ear-candy": FAQ
  • +Push Button Volume: FAQ
  • +self-boot EEPROM image: FAQ
  • +Sigma300 Family Products: FAQ
  • -SigmaDSP: FAQ
    • Booting a SigmaDSP from a microcontroller with no C compiler
    • Calculating Filter Coefficients to Store in a Microcontroller
    • Can I program multiple SigmaDSPs in parallel using one USBi?
    • Can I use SigmaDSP to decode MP3/WAV/AAC?
    • Can I write C or assembly code for SigmaDSP in SigmaStudio?
    • Can SigmaDSP do frequency-domain processing like FFT or pitch shift?
    • Can we bundle SigmaStudio with our product design?
    • Creating a delay after startup
    • Developing custom algorithms and/or using 3rd party algorithms
    • How can I estimate MIPS/Memory resource on SigmaDSP?
    • How do I create the microcontroller code to interface to my SigmaDSP?
    • How do I start a timer after power-on, or when the input signal goes away?
    • How many instructions can be executed per sample in SigmaDSP?
    • Memory requirements for booting a SigmaDSP with a microcontroller
    • Monitoring average and instantaneous signal levels
    • Playing audio samples in SigmaDSP
    • SigmaDSP PCB Layout Best Practices
    • SigmaDSP Products and Evaluation Boards - ROHS and REACH Compliance
    • SigmaStudio 3.4 Released
    • Updating SigmaDSP Parameter with a Microcontroller
    • Using two SigmaDSP evaluation boards simultaneously with one USBi board
    • Welcome to the SIGMADSP Processors and SIGMASTUDIO Development tool community
    • What are the number formats for SigmaDSP?
    • What is the step size for audio delay in a SigmaDSP?
    • What types of capacitors are good to use in the analog audio signal path?
    • Where can I buy a SigmaDSP Evaluation Board or USBi (EVAL-ADUSB2EBZ)?
    • Which SigmaDSP ICs support selfbooting from an EEPROM?
    • Which SPI Mode is used by SigmaDSP Devices?
    • Why isn't a software/documentation CD included with my evaluation board?
  • +SigmaStudio: FAQ
  • +single precision VS double precision: FAQ
  • +Stimulus-Probe Capability and Limitations: FAQ
  • +Stopwatch to Count Successive Samples: FAQ
  • +Toolbox into the schematic tab: FAQ
  • +USB communications between the PC and SigmaDSP: FAQ
  • +Using Hierarchy Boards to create re-usable code: FAQ
  • New SigmaStudio 3.2.0 beta version available
  • SigmaStudio 3.3 Released
  • SigmaStudio 3.9.2 Beta Available for Download
  • SigmaStudio Rev 3.15.2 Bug Report for SPI EEPROM Write Speed

Can I program multiple SigmaDSPs in parallel using one USBi?

Question: Can I program multiple SigmaDSPs in parallel using one USBi?

Answer: Yes, you can string together multiple SigmaDSPs on one or more PCBs and control them with a single USBi.

If all of the SigmaDSPs in the chain are running the same program, you can set them all to the same address and connect the I2C lines (SDA and SCL) in parallel to all of them.

Here's an example of where we set up 6 EVAL-ADAU1701MINIZ boards in the lab connected to a single USBi via a ribbon cable with header connectors. In this case, you set all of the SigmaDSPs to the same I2C address and use a single SigmaStudio project containing a single SigmaDSP IC. When you Link-Compile-Download, the same data will be sent to all of the SigmaDSPs on the I2C bus. As long as the cable is relatively short and the signal integrity of the signals is maintained, this works just fine.

In the case where the program needs to be different on each SigmaDSP, you need to make a SigmaStudio project with multiple ICs. You can either set different I2C addresses for each SigmaDSP, or use different SPI latches for each SigmaDSP, or use a combination of I2C and SPI simultaneously.

Here is a picture of our internal USB testing board, which contains two ADAU1701 SigmaDSPs. The communications protocol can be easily changed for each SigmaDSP between I2C or SPI, and the addresses and latch lines are also configurable.

Tags: i2c spi usbi sigmastudio SigmaDSP
  • Share
  • History
  • More
  • Cancel
 
Related Content
  • How do I self-boot multiple SigmaDSPs in a single system?
    ADIApproved
    If there are multiple SigmaDSPs in a system, they will all attempt to boot from an EEPROM at address 0xA0. How can a system with multiple SigmaDSPs use the selfboot function but have unique programs in...
  • RE: I2C communication with ADAU1466Z
    DaveThib
    Hello starkers, SPI and I2C from a hardware basis is not compatible. However, you could do this and let me explain how. The four SPI comms port pins for the DSP slave comms port goes directly to...
  • 2x SigmaDSP controlled from single SigmaStudio
    ChUmI
    Hi Guys, Can I connect two SigmaDSPs to single SigmaStudio and work with both simultaneously?... My idea is to build a system with two SigmaDSP processors and control it using single SigmaStudio environment...
 
Related Content
  • How do I self-boot multiple SigmaDSPs in a single system?
    ADIApproved
    If there are multiple SigmaDSPs in a system, they will all attempt to boot from an EEPROM at address 0xA0. How can a system with multiple SigmaDSPs use the selfboot function but have unique programs in...
  • RE: I2C communication with ADAU1466Z
    DaveThib
    Hello starkers, SPI and I2C from a hardware basis is not compatible. However, you could do this and let me explain how. The four SPI comms port pins for the DSP slave comms port goes directly to...
  • 2x SigmaDSP controlled from single SigmaStudio
    ChUmI
    Hi Guys, Can I connect two SigmaDSPs to single SigmaStudio and work with both simultaneously?... My idea is to build a system with two SigmaDSP processors and control it using single SigmaStudio environment...