Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
    • 3 Real World Methods to Make Your Power Supply More Intelligent
    View All Webinars
  • Community Hub

    Challenge Yourself!

      New KCC Quiz AQQ299 about Opamp Open Loop Gain and LTspice

      A kind proposal from Al Butvidas 1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

EngineerZone
EngineerZone
SigmaDSP Processors & SigmaStudio Dev. Tool
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
SigmaDSP Processors & SigmaStudio Dev. Tool
  • Processors & DSP
SigmaDSP Processors & SigmaStudio Dev. Tool
Documents Using the DSP Control mode of the ADAU1761 PGA / ALC
  • Q&A
  • File Uploads
  • Members
  • Tags
  • Cancel
  • Documents
  • SigmaDSP YouTube Channel - Dave Thib
  • +AD193x: FAQ
  • +ADAU1401AEBZ: FAQ
  • +ADAU144x: FAQ
  • +ADAU1452: FAQ
  • +ADAU145x: FAQ
  • +ADAU1701: FAQ
  • +ADAU1701MINIZ- FAQ
  • -ADAU1761: FAQ
    • Slow rate random number generator
    • Using the DSP Control mode of the ADAU1761 PGA / ALC
  • +ADAU1772: FAQ
  • +ADI: FAQ
  • +AN-951: FAQ
  • +bitwise logic: FAQ
  • +Compressor Table Format: FAQ
  • +Creating a simple balance crossfade control: FAQ
  • +Creating constant-dB envelope decay using an existing linear decay algorithm: FAQ
  • +Crossover with more than 3 bands: FAQ
  • +E2PROM: FAQ
  • +EEPROM: FAQ
  • +EVAL DAU144XEBZ: FAQ
  • +EVAL-ADAU1781Z: FAQ
  • +Excluding Cells from the Exported System Files: FAQ
  • +GPIO button: FAQ
  • +GPIOs or Aux ADCs: FAQ
  • +How do I execute a software safeload write?: FAQ
  • +IIR coefficient filter: FAQ
  • +IIR filter: FAQ
  • +Peak Full Range Compressor: FAQ
  • +Preserving "Ear-candy": FAQ
  • +Push Button Volume: FAQ
  • +self-boot EEPROM image: FAQ
  • +Sigma300 Family Products: FAQ
  • +SigmaDSP: FAQ
  • +SigmaStudio: FAQ
  • +single precision VS double precision: FAQ
  • +Stimulus-Probe Capability and Limitations: FAQ
  • +Stopwatch to Count Successive Samples: FAQ
  • +Toolbox into the schematic tab: FAQ
  • +USB communications between the PC and SigmaDSP: FAQ
  • +Using Hierarchy Boards to create re-usable code: FAQ
  • New SigmaStudio 3.2.0 beta version available
  • SigmaStudio 3.3 Released
  • SigmaStudio 3.9.2 Beta Available for Download
  • SigmaStudio Rev 3.15.2 Bug Report for SPI EEPROM Write Speed

Using the DSP Control mode of the ADAU1761 PGA / ALC

The ADAU1761 analog front end has an ALC (automatic level control) function that sets the gain of the differential input paths dynamically, based on the level of the incoming signals. However, the ALC can be bypassed and the DSP program can directly control the amount of gain applied to the differential inputs.

In order to do this, the differential path for one or both channels needs to be Enabled and Unmuted. The LDBOOST (and/or RDBOOST) should also be set to either 0 dB or 20 dB as needed, in order to enable the differential path.

Then, the ALCSEL bits should be set to DSP Control mode.

Now, in the DSP program schematic, the user can add AIGC Output cells to the project:

Channel 0 maps to the left PGA.

Channel 1 maps to the right PGA.

Now, the 5.23 signal that is fed to each of these cells determines the gain of the corresponding PGAs.

As a simple example, to set the gain of each PGA to 0.5 (or -6 dB), create a DC Input Entry cell from the Sources library and set it to 0.5, then wire it to the AIGC outputs.

In the next example, a Sine Tone at 10 Hz is scaled and shifted using the Multiply and Add cells so that it ranges between 0 and 1, and then it is sent to the AIGC Output cells. This causes the PGA gain to shift rapidly back and forth between 0 dB and muted, which creates a tremolo effect.

In the following example, the peak level of each input is detected by the Peak Envelope cells, and the inverse of this signal is created using the Divide cells and a DC Input Entry cell. The result is sent to the AIGC Output cells. This means that the inverse of the peak level of the input is used to scale the PGA gain. The result is that the gain is high when the input signal is low, but the gain is lowered to avoid clipping when the input level increases.

These are just a few examples of what can be done using DSP Control mode on the ADAU1761's PGAs.

Tags: dsp control pga adau1761
  • Share
  • History
  • More
  • Cancel
 
Related Content
  • RE: Automatic Level Control (ALC) of ADAU1761
    ADIApproved
    The ALC controls the gain in the PGA, so it can only be used with differential or pseudo-differential inputs. This is described in the first column on page 32 of the datasheet. When ALCSEL is set to...
  • RE: ADAU1361, ADAU1761 - input differential level
    ADIApproved
    If you input the datasheet's defined full-scale input, which is 2.83 Vp-p centered around CM which is 3.3/2, then you should see a peak level of 1.0 (in 5.23 format) in the DSP. This 1.0 value can be read...
  • ADAU1761 DSP control of PGA
    PaulBKaraoke
    I have been using the ALC in the register section and it works great. I just realized that the detect does not not work independently when both channels are active together (stereo mode) So I would like...
 
Related Content
  • RE: Automatic Level Control (ALC) of ADAU1761
    ADIApproved
    The ALC controls the gain in the PGA, so it can only be used with differential or pseudo-differential inputs. This is described in the first column on page 32 of the datasheet. When ALCSEL is set to...
  • RE: ADAU1361, ADAU1761 - input differential level
    ADIApproved
    If you input the datasheet's defined full-scale input, which is 2.83 Vp-p centered around CM which is 3.3/2, then you should see a peak level of 1.0 (in 5.23 format) in the DSP. This 1.0 value can be read...
  • ADAU1761 DSP control of PGA
    PaulBKaraoke
    I have been using the ALC in the register section and it works great. I just realized that the detect does not not work independently when both channels are active together (stereo mode) So I would like...