• LiDAR Solutions
    • Motor Control Hardware Platforms
    • Speech Processing Solutions
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
    Accelerate RF Subsystem Integration with COTS SoMs and Phased Array Solutions. As building a subsystem from early prototype to full deployment is never...
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
      KCC's Quizzes AQQ301 - Counting Bicycles and Tricycles

      1. Quote of the month: " People who didn't need people needed people around to know that they were the kind of people who didn't need people" - Terry Pratchett...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 2: Achieving Phase Repeatability

    This article discusses a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a...

EngineerZone
EngineerZone
SigmaDSP Processors & SigmaStudio Dev. Tool
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
SigmaDSP Processors & SigmaStudio Dev. Tool
  • Processors & DSP
SigmaDSP Processors & SigmaStudio Dev. Tool
Documents Setting the PLL mode for the ADAU1701 at different sample rates
  • Q&A
  • Docs/FAQs
  • File Uploads
  • Members
  • Tags
  • Cancel
  • Documents
  • SigmaDSP YouTube Channel - Dave Thib
  • +AD193x: FAQ
  • +ADAU1401AEBZ: FAQ
  • +ADAU144x: FAQ
  • +ADAU1452: FAQ
  • +ADAU145x: FAQ
  • -ADAU1701: FAQ
    • ADAU1701 Input and Output Signal Routing
    • ADAU1701: ADC resistor values for higher sample rates
    • Implementing Safeload Writes on the ADAU1701
    • My 2IN4OUT Proto with SPDIF based on ADAU1701
    • Setting the PLL mode for the ADAU1701 at different sample rates
    • Thoughts on using index selectable filters...
    • Using hardware data capture (trap) registers with the DSP Readback cell (AD1940, ADAU1701)
  • +ADAU1701MINIZ- FAQ
  • +ADAU1761: FAQ
  • +ADAU1772: FAQ
  • +ADI: FAQ
  • +AN-951: FAQ
  • +bitwise logic: FAQ
  • +Compressor Table Format: FAQ
  • +Creating a simple balance crossfade control: FAQ
  • +Creating constant-dB envelope decay using an existing linear decay algorithm: FAQ
  • +Crossover with more than 3 bands: FAQ
  • +E2PROM: FAQ
  • +EEPROM: FAQ
  • +EVAL DAU144XEBZ: FAQ
  • +EVAL-ADAU1781Z: FAQ
  • +Excluding Cells from the Exported System Files: FAQ
  • +GPIO button: FAQ
  • +GPIOs or Aux ADCs: FAQ
  • +How do I execute a software safeload write?: FAQ
  • +IIR coefficient filter: FAQ
  • +IIR filter: FAQ
  • +Peak Full Range Compressor: FAQ
  • +Preserving "Ear-candy": FAQ
  • +Push Button Volume: FAQ
  • +self-boot EEPROM image: FAQ
  • +Sigma300 Family Products: FAQ
  • +SigmaDSP: FAQ
  • +SigmaStudio: FAQ
  • +single precision VS double precision: FAQ
  • +Stimulus-Probe Capability and Limitations: FAQ
  • +Stopwatch to Count Successive Samples: FAQ
  • +Toolbox into the schematic tab: FAQ
  • +USB communications between the PC and SigmaDSP: FAQ
  • +Using Hierarchy Boards to create re-usable code: FAQ
  • New SigmaStudio 3.2.0 beta version available
  • SigmaStudio 3.3 Released
  • SigmaStudio 3.9.2 Beta Available for Download
  • SigmaStudio Rev 3.15.2 Bug Report for SPI EEPROM Write Speed

Setting the PLL mode for the ADAU1701 at different sample rates

     The 1701 's fundamental clock is the MIPS clock, which always operates at 49.152 MHz (roughly 50 MIPS) for any "standard" sample rate (48 / 96 / 192 KHz).  The only exception is 44.1 KHz and its multiples, in that case the chip runs about 8% slower, at 45.1584 MIPS.  You're running a standard sample rate (192 KHz), so your -1701 operates at 49.152 MHz.

     As you know, the base 48K sample rate allows for 1024 instructions.  48000 times 1024 equals -- guess what, the 49.152 MIPS rate.  Switching to  192 KHz allows for only 256 instructions, because 256 x 192000 still equals 49.152 MHz.  The chip doesn't run any faster, so you must trade off some program capacity for sample rate.  You set the tradeoff in SigmaStudio's hardware config screen, which in turn sets the core control register in the -1701.  No hardware pins change at all.  That's why your eval board, with its 12.288 MHz crystal, PLLMODE0 = GND and PLLMODE1=3.3V, can run at any of the standard sample rates.

     What the PLLMODE0 and PLLMODE1 pins allow for is the use of different external clock frequencies if desired.  This directly sets the PLL multiplier, so the MIPS clock remains at roughly 50 MIPS with the different MCLK inputs.  Figure 12 on page 18 of the ADAU1701 data sheet would be a bit less confusing if set up as below:

Note that earlier on Page 18, ADI recommends that when using the crystal oscillator, you always  use a 12.288 MHz crystal for standard rates (or 11.2896 MHz for 44.1 KHz rate).  To get your ~50 MIPS clock, you set  PLLMODE0 to 0 & PLLMODE1 to 1 which runs the PLL at MCLK x 4. (or 256 x 48000).  Thus, when using the internal crystal oscillator, there's no need to deviate from what's on the evaluation board -- whether your sample rate is 48, 96, or 192 KHz.

     Best regards,

     Bob

This FAQ was generated from the following discussion: a dummy question about pll in 1701

Tags: adau1702 adau1401 clock configuration pll adau1701 Show More
  • Share
  • History
  • More
  • Cancel
 
Related Content
  • RE: a dummy question about pll in 1701
    KJBob
    Hello Skfir, As my friend Mike says, there's no dumb questions (sometimes there's dumb answers, and I hope this isn't one of them). The 1701 's fundamental clock is the MIPS clock, which always operates...
  • RE: Adau1701 - Doubt about level input and sample rate
    KJBob
    Hello Francis, 1. The ADAU1701's ADCs are current-sensing, so the external series resistors set their sensitivity. Just choose the resistor value that provides the desired full-scale input for your application...
  • RE: ADAU1701 - Sample Rate Issues
    KJBob
    Hello, The short answer is, Set your PLL mode to "256 x Fs" -- that is, PLL_MODE_0 low, and PLL_MODE_1 high -- and you'll be operating correctly. What the PLL really does is derive the 4 9.152 MHz...
 
Related Content
  • RE: a dummy question about pll in 1701
    KJBob
    Hello Skfir, As my friend Mike says, there's no dumb questions (sometimes there's dumb answers, and I hope this isn't one of them). The 1701 's fundamental clock is the MIPS clock, which always operates...
  • RE: Adau1701 - Doubt about level input and sample rate
    KJBob
    Hello Francis, 1. The ADAU1701's ADCs are current-sensing, so the external series resistors set their sensitivity. Just choose the resistor value that provides the desired full-scale input for your application...
  • RE: ADAU1701 - Sample Rate Issues
    KJBob
    Hello, The short answer is, Set your PLL mode to "256 x Fs" -- that is, PLL_MODE_0 low, and PLL_MODE_1 high -- and you'll be operating correctly. What the PLL really does is derive the 4 9.152 MHz...