Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
    • COTS SoMs & Phased Array Solutions for Rapid RF Subsystem Integration
    • LEO Satcom: Application of RF, Mixed-Signal, & Beamforming ICs
    • 3 Real World Methods to Make Your Power Supply More Intelligent
    • Revolutionizing Flow Cytometry: 20-Bit Precision Signal Chain
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC's Quiz AQQ300 about Divisibility by 6

      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Clock Tree Design and Why “PLL Locked” Is Not Enough

    In high-performance RF systems, clocking architecture is a foundational element that directly governs signal integrity, synchronization, and overall system...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Improving Industrial Functional Safety Compliance with High Performance Supervisory CircuitsPart 5: Sequencers Eliminate Systematic Failures

    This article shifts focus from managing the quantitative metrics of functional safety toward mastering the qualitative yet equally critical challenge:...

EngineerZone
EngineerZone
SigmaDSP Processors & SigmaStudio Dev. Tool
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
SigmaDSP Processors & SigmaStudio Dev. Tool
  • Processors & DSP
SigmaDSP Processors & SigmaStudio Dev. Tool
Documents SigmaStudio 3.3 Released
  • Q&A
  • File Uploads
  • Members
  • Tags
  • Cancel
  • Documents
  • SigmaDSP YouTube Channel - Dave Thib
  • +AD193x: FAQ
  • +ADAU1401AEBZ: FAQ
  • +ADAU144x: FAQ
  • +ADAU1452: FAQ
  • +ADAU145x: FAQ
  • +ADAU1701: FAQ
  • +ADAU1701MINIZ- FAQ
  • +ADAU1761: FAQ
  • +ADAU1772: FAQ
  • +ADI: FAQ
  • +AN-951: FAQ
  • +bitwise logic: FAQ
  • +Compressor Table Format: FAQ
  • +Creating a simple balance crossfade control: FAQ
  • +Creating constant-dB envelope decay using an existing linear decay algorithm: FAQ
  • +Crossover with more than 3 bands: FAQ
  • +E2PROM: FAQ
  • +EEPROM: FAQ
  • +EVAL DAU144XEBZ: FAQ
  • +EVAL-ADAU1781Z: FAQ
  • +Excluding Cells from the Exported System Files: FAQ
  • +GPIO button: FAQ
  • +GPIOs or Aux ADCs: FAQ
  • +How do I execute a software safeload write?: FAQ
  • +IIR coefficient filter: FAQ
  • +IIR filter: FAQ
  • +Peak Full Range Compressor: FAQ
  • +Preserving "Ear-candy": FAQ
  • +Push Button Volume: FAQ
  • +self-boot EEPROM image: FAQ
  • +Sigma300 Family Products: FAQ
  • +SigmaDSP: FAQ
  • +SigmaStudio: FAQ
  • +single precision VS double precision: FAQ
  • +Stimulus-Probe Capability and Limitations: FAQ
  • +Stopwatch to Count Successive Samples: FAQ
  • +Toolbox into the schematic tab: FAQ
  • +USB communications between the PC and SigmaDSP: FAQ
  • +Using Hierarchy Boards to create re-usable code: FAQ
  • New SigmaStudio 3.2.0 beta version available
  • SigmaStudio 3.3 Released
  • SigmaStudio 3.9.2 Beta Available for Download
  • SigmaStudio Rev 3.15.2 Bug Report for SPI EEPROM Write Speed

SigmaStudio 3.3 Released

SigmaStudio 3.3 Released by ADIApproved

SigmaStudio 3.3 is now available from the download page on analog.com. The biggest new feature is that this version now fully supports Windows 7, both 32-bit (x86) and 64-bit versions. Separate installers for each version are included in the download file. The full list of enhancements in version 3.3 includes the items in the list below. This can also be found in the readme file included in the installation.

  • Windows      Vista and Windows 7 x64 support.
  • New      installation process:
    • Default       Installation file path location for x64 architecture is Program Files       (x64).
    • Default       SigmaStudio projects including the “Sample Schematics” path location is       \<users>\Documents\Analog Devices\SigmaStudio <version>\Projects.
    • Addins.xml       default path is AppData\Roaming\Analog Devices\SigmaStudio <version>      
    • During       installation process, the user will be prompted with an additional USBi       installation. This is to install the right USBi drivers into the current       machine and it only needs to be run once.
  • PLL      wait command during “download-compile”.
  • Export      uC files with the wait command. This includes Sequencer support on wait      command.
  • Envelope      time span from 10 ms to 4400 ms.
  • Peaking      No Post Gain now supports full range (-90 dB -> +24 dB).
  • New SigmaDSP      Gen3 volume controls (Linear Gain, RC Gain optimized, dB, and dB compact).
  • ADAU1701      Assembler modification to better display MIPS used at design time.
  • Additions      and updates to Gen3 core assemblers.
  • Addition of NoiseReduction algorithm to standard library
  • Addition of SuperBass algorithm to standard library
  • Increase of Index Lookup Table size to 500 from 100


RE: SigmaStudio 3.3 Released by embedded.hardware:

Hi All

My last use of Sigma Studio was 3.0, So...

I've download this release and I navigate from component list.

I didn't find any informations about the Automatic Volume Control (Unclassified Section).

Should you explain me how it works ? Why the help do not show all componentes listed ?

Regards

Karim Mouhamed

Embedded Hardware


RE: SigmaStudio 3.3 Released by inventis:

Hi,

The last week I made some automatic updates from windows in my Win7 64bit

Today when I try to run sigmastudio 3.3 the program crash.

Anyone has a similar problem?

Regards


RE: SigmaStudio 3.3 Released by ADIApproved:

Please see the message at the top of the SigmaDSP forum. There is a known problem with SigmaStudio running in Windows 7 SP1. We are aware of this and it will be fixed in an upcoming release.


RE: SigmaStudio 3.3 Released by inventis:

Any idea about the scheduling for a bug fixed release of SigmaStudio ?


RE: SigmaStudio 3.3 Released by mys:

The download page for SigmaStudio shows that versions 3.3.2 (Beta) and 3.3.0 (Current Release) are available. However, selecting the Beta option leads to a page with the message "File not found". The URL shows "SigmaStudio3_3_2_Beta.zip" as the target filename. Is the Beta version still available for download?


RE: SigmaStudio 3.3 Released by ADIApproved:

It looks like there was a mix-up on the download site, but now you should see version 3.4 available. Try the release version. It still shows "beta" in the splash screen for some reason - I'll tell the software team about this.

Tags: Audio Signal Processors SigmaDSP Audio Processors adau1701