• LiDAR Solutions
    • Motor Control Hardware Platforms
    • Speech Processing Solutions
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
    Accelerate RF Subsystem Integration with COTS SoMs and Phased Array Solutions. As building a subsystem from early prototype to full deployment is never...
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
      KCC's Quizzes AQQ301 - Counting Bicycles and Tricycles

      1. Quote of the month: " People who didn't need people needed people around to know that they were the kind of people who didn't need people" - Terry Pratchett...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 2: Achieving Phase Repeatability

    This article discusses a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a...

EngineerZone
EngineerZone
SigmaDSP Processors & SigmaStudio Dev. Tool
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
SigmaDSP Processors & SigmaStudio Dev. Tool
  • Processors & DSP
SigmaDSP Processors & SigmaStudio Dev. Tool
Documents New SigmaStudio 3.2.0 beta version available
  • Q&A
  • Docs/FAQs
  • File Uploads
  • Members
  • Tags
  • Cancel
  • Documents
  • SigmaDSP YouTube Channel - Dave Thib
  • +AD193x: FAQ
  • +ADAU1401AEBZ: FAQ
  • +ADAU144x: FAQ
  • +ADAU1452: FAQ
  • +ADAU145x: FAQ
  • +ADAU1701: FAQ
  • +ADAU1701MINIZ- FAQ
  • +ADAU1761: FAQ
  • +ADAU1772: FAQ
  • +ADI: FAQ
  • +AN-951: FAQ
  • +bitwise logic: FAQ
  • +Compressor Table Format: FAQ
  • +Creating a simple balance crossfade control: FAQ
  • +Creating constant-dB envelope decay using an existing linear decay algorithm: FAQ
  • +Crossover with more than 3 bands: FAQ
  • +E2PROM: FAQ
  • +EEPROM: FAQ
  • +EVAL DAU144XEBZ: FAQ
  • +EVAL-ADAU1781Z: FAQ
  • +Excluding Cells from the Exported System Files: FAQ
  • +GPIO button: FAQ
  • +GPIOs or Aux ADCs: FAQ
  • +How do I execute a software safeload write?: FAQ
  • +IIR coefficient filter: FAQ
  • +IIR filter: FAQ
  • +Peak Full Range Compressor: FAQ
  • +Preserving "Ear-candy": FAQ
  • +Push Button Volume: FAQ
  • +self-boot EEPROM image: FAQ
  • +Sigma300 Family Products: FAQ
  • +SigmaDSP: FAQ
  • +SigmaStudio: FAQ
  • +single precision VS double precision: FAQ
  • +Stimulus-Probe Capability and Limitations: FAQ
  • +Stopwatch to Count Successive Samples: FAQ
  • +Toolbox into the schematic tab: FAQ
  • +USB communications between the PC and SigmaDSP: FAQ
  • +Using Hierarchy Boards to create re-usable code: FAQ
  • New SigmaStudio 3.2.0 beta version available
  • SigmaStudio 3.3 Released
  • SigmaStudio 3.9.2 Beta Available for Download
  • SigmaStudio Rev 3.15.2 Bug Report for SPI EEPROM Write Speed

New SigmaStudio 3.2.0 beta version available

New SigmaStudio 3.2.0 beta version available by ADIApproved

There is a new beta, version 3.2, of SigmaStudio available on the software's download page. This version should not be used for production designs, but rather to preview bug fixes and new features that will be available in the next release. Please feel free to download this version and report any bugs (or things you like!) in the thread below.

The release information for this version includes:

Enhancements in SigmaStudio 3.2.0

  • SigmaStudio opens faster due to code optimization.
  • TreeToolBox now displays Algorithm Description.
  • New Standard Peaking Dynamics Processors.
  • New Standard Independent Channel Linked/Unlinked Dynamics Processors.
  • Added the following new algorithms/modules
    • Voice Activity Detector (VAD) Standard (ADAU144x, ADAU176x, ADAU178x)
    • Voice Activity Detector (VAD) With Acceleration (ADAU144x, ADAU176x, ADAU178x)
    • Endless Loop Chime (AD1940, ADAU170x, ADAU144x, ADAU176x, ADAU178x)
  • SigmaStudio A/B comparison download time enhanced.
  • Implementation of CRC and Watchdog for ADAU144x.

 

SigmaStudio 3.2.0 Major Bug Fixes

  • Label position bug on save/open fixed.
  • Addins Browser Installer error message upon adding a valid Dll fixed.
  • Chime time/frequency controls now update the algorithm slope.
  • Changed the Chime min and max time.
  • Compressor  Graph UI serialization on first point fixed.
  • GUI add/remove drag-point errors were fixed for all chime and envelope algorithms. Misbehavior of the points was      also fixed.
  • TreeToolBox “Unclassified” Folder with multiple listings issue was corrected.
  • Parametric EQ
    • Additional Filter bug upon modifying X-min axis fixed.
    • SpinText color upon bug on enable/disable fixed.
  • Dejitter window register bug fixed for ADAU1381, ADAU 178x and ADAU1x61
  • Standard Independent RMS Dynamics Processor Algorithm:
    • Attack and Release controls now are updating its value every time they get modified.
    • Compression Visualization issue fixed.
  • Mono MUX No Slew: Changed the algorithm numbering system to avoid duplicate addresses.
  • Sequencer Window Export Files: Exports files with the right number of address bytes for ICs that have address bytes different than two.


RE: New SigmaStudio 3.2.0 beta version available by ADIApproved:

No, SigmaStudio is not yet supported in Windows 7. This FAQ will be updated when a Windows 7-compatible version is available.


RE: New SigmaStudio 3.2.0 beta version available by MagicRuB:

Any chance does Sigma Studio 3.2.0 work on Windows 7 x64?


RE: New SigmaStudio 3.2.0 beta version available by MagicRuB:

possible x64 solution: https://ez.analog.com/message/14067


RE: New SigmaStudio 3.2.0 beta version available by ruchi.singh2005@gmail.com:

Any chance does Sigma Studio 3.2.0 work on BD-SL-i.MX6 board which is anARM Cortex-A9 based Linux evaluation platform.


RE: New SigmaStudio 3.2.0 beta version available by Yagami:

Hi ruchi.singh2005,

SigmaStudio version 3.2.0 is almost 4 years old and is no longer supported. I would suggest keeping up to date with the latest version, which you can download here:

New SigmaStudio Download Site

Tags: adau1381 Integrated/Special Purpose A/D Converters Audio CODECs