Accelerate RF Subsystem Integration with COTS SoMs and Phased Array Solutions. As building a subsystem from early prototype to full deployment is never...
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
      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 2: Achieving Phase Repeatability

    This article discusses a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a...

EngineerZone
EngineerZone
SigmaDSP Processors & SigmaStudio Dev. Tool
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
SigmaDSP Processors & SigmaStudio Dev. Tool
  • Processors & DSP
SigmaDSP Processors & SigmaStudio Dev. Tool
Documents SigmaStudio Rev 3.15.2 Bug Report for SPI EEPROM Write Speed
  • Q&A
  • Docs/FAQs
  • File Uploads
  • Members
  • Tags
  • Cancel
  • Documents
  • SigmaDSP YouTube Channel - Dave Thib
  • +AD193x: FAQ
  • +ADAU1401AEBZ: FAQ
  • +ADAU144x: FAQ
  • +ADAU1452: FAQ
  • +ADAU145x: FAQ
  • +ADAU1701: FAQ
  • +ADAU1701MINIZ- FAQ
  • +ADAU1761: FAQ
  • +ADAU1772: FAQ
  • +ADI: FAQ
  • +AN-951: FAQ
  • +bitwise logic: FAQ
  • +Compressor Table Format: FAQ
  • +Creating a simple balance crossfade control: FAQ
  • +Creating constant-dB envelope decay using an existing linear decay algorithm: FAQ
  • +Crossover with more than 3 bands: FAQ
  • +E2PROM: FAQ
  • +EEPROM: FAQ
  • +EVAL DAU144XEBZ: FAQ
  • +EVAL-ADAU1781Z: FAQ
  • +Excluding Cells from the Exported System Files: FAQ
  • +GPIO button: FAQ
  • +GPIOs or Aux ADCs: FAQ
  • +How do I execute a software safeload write?: FAQ
  • +IIR coefficient filter: FAQ
  • +IIR filter: FAQ
  • +Peak Full Range Compressor: FAQ
  • +Preserving "Ear-candy": FAQ
  • +Push Button Volume: FAQ
  • +self-boot EEPROM image: FAQ
  • +Sigma300 Family Products: FAQ
  • +SigmaDSP: FAQ
  • +SigmaStudio: FAQ
  • +single precision VS double precision: FAQ
  • +Stimulus-Probe Capability and Limitations: FAQ
  • +Stopwatch to Count Successive Samples: FAQ
  • +Toolbox into the schematic tab: FAQ
  • +USB communications between the PC and SigmaDSP: FAQ
  • +Using Hierarchy Boards to create re-usable code: FAQ
  • New SigmaStudio 3.2.0 beta version available
  • SigmaStudio 3.3 Released
  • SigmaStudio 3.9.2 Beta Available for Download
  • SigmaStudio Rev 3.15.2 Bug Report for SPI EEPROM Write Speed

SigmaStudio Rev 3.15.2 Bug Report for SPI EEPROM Write Speed

SigmaStudio Rev 3.15.2 Bug Report for SPI EEPROM Write Speed by DaveThib

Hello EngineerZone community,

There is a bug that was introduced with SigmaStudio revision 3.15.2 released and beta versions. This bug was not on earlier revisions and will be fixed on the next revision.

The symptoms are that after writing the program to the EEPROM and then booting up from the EERPOM, the program takes a very long time to load! An average program was taking about 45 seconds to load. So what happens is that you reset the DSP and then it seems like the writing to the EEPROM failed because you do not see the program running. Not realizing you have to wait a very long time for the program to run!

As far as I know this is only seen with the ADAU1452/1451/1450 family of parts. It is only when using SPI for booting.

The program will ignore the Write Speed entry in the  EEPROM Properties page. The actual write speed will be around 6kHz!

There is a workaround. Most users set it to a 1MHz write speed. So you can manually edit the hex file and change the write speed. Then burn that into the EEPROM or just go directly into the EEPROM, if you can, and write in new values. If you try to directly write to the EEPROM you will have to hold the DSP in reset to tri-state the SPI master port.

Figure 39 in the datasheet, "Self boot EEPROM Header Format" shows the header and shows the last four bytes of the 16 byte header is the EEPROM write speed. What I found is that it was writing 0x00, 0x9D, 0x2F and 0x35.

Change these four bytes to: 0x01, 0xC2, 0x01, 0x01 and you will find it boots up much faster!

Add to this discussion if you found this issue with other  processors. The next released revision will have a fix for this problem.

Dave T

Tags: eeprom