Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp Open Loop Gain and LTspice

      A kind proposal from Al Butvidas 1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

EngineerZone
EngineerZone
SigmaDSP Processors & SigmaStudio Dev. Tool
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
SigmaDSP Processors & SigmaStudio Dev. Tool
  • Processors & DSP
SigmaDSP Processors & SigmaStudio Dev. Tool
Documents Sigma 300 (ADAU145x) Exponential Slewing
  • Q&A
  • File Uploads
  • Members
  • Tags
  • Cancel
  • Documents
  • SigmaDSP YouTube Channel - Dave Thib
  • +AD193x: FAQ
  • +ADAU1401AEBZ: FAQ
  • +ADAU144x: FAQ
  • +ADAU1452: FAQ
  • +ADAU145x: FAQ
  • +ADAU1701: FAQ
  • +ADAU1701MINIZ- FAQ
  • +ADAU1761: FAQ
  • +ADAU1772: FAQ
  • +ADI: FAQ
  • +AN-951: FAQ
  • +bitwise logic: FAQ
  • +Compressor Table Format: FAQ
  • +Creating a simple balance crossfade control: FAQ
  • +Creating constant-dB envelope decay using an existing linear decay algorithm: FAQ
  • +Crossover with more than 3 bands: FAQ
  • +E2PROM: FAQ
  • +EEPROM: FAQ
  • +EVAL DAU144XEBZ: FAQ
  • +EVAL-ADAU1781Z: FAQ
  • +Excluding Cells from the Exported System Files: FAQ
  • +GPIO button: FAQ
  • +GPIOs or Aux ADCs: FAQ
  • +How do I execute a software safeload write?: FAQ
  • +IIR coefficient filter: FAQ
  • +IIR filter: FAQ
  • +Peak Full Range Compressor: FAQ
  • +Preserving "Ear-candy": FAQ
  • +Push Button Volume: FAQ
  • +self-boot EEPROM image: FAQ
  • +Sigma300 Family Products: FAQ
  • +SigmaDSP: FAQ
  • -SigmaStudio: FAQ
    • Can I have multiple versions of SigmaStudio installed simultaneously?
    • How are the audio inputs routed in SigmaStudio's Input cell?
    • How can I change parameters on-the-fly in an application without SigmaStudio?
    • How do I change the sample rate of my SigmaStudio system?
    • How do I report a SigmaStudio bug?
    • New SigmaStudio 3.3 Beta Version Available
    • New SigmaStudio Download Site
    • Sigma 300 (ADAU145x) Exponential Slewing
    • SigmaStudio consulting services...
    • The ADAU1372 is not on the list of compatible processors or under Processors/DSPs on Sigmastudio 3.11.1 or 3.11. Can you please tell me how I can use the EVAL board with ADAU1372?
    • Third Party Algorithm Plugins in SigmaStudio
    • True peak-to-peak detection in SigmaStudio
    • Using compressors to avoid output clipping
    • Using stopwatch with feedback loop to create periodic test signal
    • What operating systems are supported to run SigmaStudio?
    • Where can I download SigmaStudio?
    • Where can I find a description of the changes made in the latest version of SigmaStudio?
    • Where can I send my questions I don't want to post in a public forum?
    • Why can't I control any of the knobs or sliders in my SigmaStudio project?
  • +single precision VS double precision: FAQ
  • +Stimulus-Probe Capability and Limitations: FAQ
  • +Stopwatch to Count Successive Samples: FAQ
  • +Toolbox into the schematic tab: FAQ
  • +USB communications between the PC and SigmaDSP: FAQ
  • +Using Hierarchy Boards to create re-usable code: FAQ
  • New SigmaStudio 3.2.0 beta version available
  • SigmaStudio 3.3 Released
  • SigmaStudio 3.9.2 Beta Available for Download
  • SigmaStudio Rev 3.15.2 Bug Report for SPI EEPROM Write Speed

Sigma 300 (ADAU145x) Exponential Slewing

  The ADAU1452's toolbox contains a External Slew Volume block with more slew choices compared to those of previous SigmaDSPs.  Its  RC and Linear slew rates are described at https://ez.analog.com/message/165526#165526

The Exponential slew has some unique characteristics, explored below.

    Rise Time

    A given slew number sets up the corresponding dB/s exponential rise shown in the table below.  This rise abruptly stops when the block's gain reaches the new input set-point.  The chart below shows slew times for a 1% to 10% rise, as well as a 10% to 90% rise, where 100% is unity gain.  For a given slew number, the times depend only upon your gain interval -- in other words, you'll get the same 10% -- 90% slew time whether your input jumps from 0.1 to 0.9, or if your input jumps from 0 to 0.9 and you begin timing as the rising gain crosses 0.1.

    This leaves the Start -- 1% measurements as an interesting special case.  Here  the input and gain both begin at zero.  Timing begins when the input jumps to 1, and ends when the block's gain reaches 1%.  An exponential rise from zero remains at zero, so in theory this slew should take forever.  In practice, the block slews from 0 to 0.01 in a finite (though quite long) time.

    Fall Time

    When the block's control input drops from any value to zero, the resulting gain characteristic is identical to that of the RC fall (which is also an exponential decay).  However, you'll find different results when the control input drops to a nonzero value.  For example, compare the RC to the exponential slew when the control input drops from 1 to 0.5 below:

    The RC slew acts exactly as a resistor-capacitor circuit.  The exponential fall, however, always follows its characteristic fall to zero, as suggested by the thin red curve shown.  It abruptly stops when falling gain reaches the input set-point.  Thus, when making a small input drop the exponential curve appears almost linear, and the resulting gain fall measures faster than with the RC choice.  To predict the fall time Dt for a fall from y1 to y2 from an original level y0, start with the time constant T from the RC chart at https://ez.analog.com/message/165526#165526.  Then calculate the fall time:  tfall  =  T x [ ln(y1/y0) - ln(y2/y0) ]