Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp Open Loop Gain and LTspice

      A kind proposal from Al Butvidas 1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

EngineerZone
EngineerZone
SigmaDSP Processors & SigmaStudio Dev. Tool
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
SigmaDSP Processors & SigmaStudio Dev. Tool
  • Processors & DSP
SigmaDSP Processors & SigmaStudio Dev. Tool
Documents New SigmaStudio 3.3 Beta Version Available
  • Q&A
  • File Uploads
  • Members
  • Tags
  • Cancel
  • Documents
  • SigmaDSP YouTube Channel - Dave Thib
  • +AD193x: FAQ
  • +ADAU1401AEBZ: FAQ
  • +ADAU144x: FAQ
  • +ADAU1452: FAQ
  • +ADAU145x: FAQ
  • +ADAU1701: FAQ
  • +ADAU1701MINIZ- FAQ
  • +ADAU1761: FAQ
  • +ADAU1772: FAQ
  • +ADI: FAQ
  • +AN-951: FAQ
  • +bitwise logic: FAQ
  • +Compressor Table Format: FAQ
  • +Creating a simple balance crossfade control: FAQ
  • +Creating constant-dB envelope decay using an existing linear decay algorithm: FAQ
  • +Crossover with more than 3 bands: FAQ
  • +E2PROM: FAQ
  • +EEPROM: FAQ
  • +EVAL DAU144XEBZ: FAQ
  • +EVAL-ADAU1781Z: FAQ
  • +Excluding Cells from the Exported System Files: FAQ
  • +GPIO button: FAQ
  • +GPIOs or Aux ADCs: FAQ
  • +How do I execute a software safeload write?: FAQ
  • +IIR coefficient filter: FAQ
  • +IIR filter: FAQ
  • +Peak Full Range Compressor: FAQ
  • +Preserving "Ear-candy": FAQ
  • +Push Button Volume: FAQ
  • +self-boot EEPROM image: FAQ
  • +Sigma300 Family Products: FAQ
  • +SigmaDSP: FAQ
  • -SigmaStudio: FAQ
    • Can I have multiple versions of SigmaStudio installed simultaneously?
    • How are the audio inputs routed in SigmaStudio's Input cell?
    • How can I change parameters on-the-fly in an application without SigmaStudio?
    • How do I change the sample rate of my SigmaStudio system?
    • How do I report a SigmaStudio bug?
    • New SigmaStudio 3.3 Beta Version Available
    • New SigmaStudio Download Site
    • Sigma 300 (ADAU145x) Exponential Slewing
    • SigmaStudio consulting services...
    • The ADAU1372 is not on the list of compatible processors or under Processors/DSPs on Sigmastudio 3.11.1 or 3.11. Can you please tell me how I can use the EVAL board with ADAU1372?
    • Third Party Algorithm Plugins in SigmaStudio
    • True peak-to-peak detection in SigmaStudio
    • Using compressors to avoid output clipping
    • Using stopwatch with feedback loop to create periodic test signal
    • What operating systems are supported to run SigmaStudio?
    • Where can I download SigmaStudio?
    • Where can I find a description of the changes made in the latest version of SigmaStudio?
    • Where can I send my questions I don't want to post in a public forum?
    • Why can't I control any of the knobs or sliders in my SigmaStudio project?
  • +single precision VS double precision: FAQ
  • +Stimulus-Probe Capability and Limitations: FAQ
  • +Stopwatch to Count Successive Samples: FAQ
  • +Toolbox into the schematic tab: FAQ
  • +USB communications between the PC and SigmaDSP: FAQ
  • +Using Hierarchy Boards to create re-usable code: FAQ
  • New SigmaStudio 3.2.0 beta version available
  • SigmaStudio 3.3 Released
  • SigmaStudio 3.9.2 Beta Available for Download
  • SigmaStudio Rev 3.15.2 Bug Report for SPI EEPROM Write Speed

New SigmaStudio 3.3 Beta Version Available

New SigmaStudio 3.3 Beta Version Available by JeradL

There is a new beta, version 3.2, of SigmaStudio available on the software's download page. The most significant update included in this version is support for both the Windows 7 OS and x64 (Vista and 7) processors. This version should not be used for production designs, but rather to preview bug fixes and new features that will be available in the next release. Please feel free to download this version and report any bugs (or things you like!) in the thread below. The download file includes installers for both x86 (32-bit) and x64 (64-bit) versions; please choose the appropriate one for your PC.

The release information for this version includes:

Enhancements in SigmaStudio 3.3.0

  • Windows      Vista and Windows 7 x64 support.
  • New      installation process:
    • Default       Installation file path location for x64 architecture is Program Files       (x64).
    • Default       SigmaStudio projects path location is \<users>\Documents\Analog       Devices\SigmaStudio\Projects.
    • During       installation process, the user will be prompted with an additional USBi       installation. This is to install the right USBi drivers into the current       machine and it only needs to be run once.
  • PLL      wait command during “download-compile”.
  • Export      uC files with the wait command. This includes Sequencer support on wait      command.
  • Envelope      time span from 10 ms to 4400 ms.
  • Peaking      No Post Gain now supports full range.


RE: New SigmaStudio 3.3 Beta Version Available by JeradL:

Note that in order to install SigmaStudio, you should double-click on the setup.exe file in the .zip download, not Sigma Studio.msi.