Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp Open Loop Gain and LTspice

      A kind proposal from Al Butvidas 1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

EngineerZone
EngineerZone
SigmaDSP Processors & SigmaStudio Dev. Tool
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
SigmaDSP Processors & SigmaStudio Dev. Tool
  • Processors & DSP
SigmaDSP Processors & SigmaStudio Dev. Tool
Documents Using two SigmaDSP evaluation boards simultaneously with one USBi board
  • Q&A
  • File Uploads
  • Members
  • Tags
  • Cancel
  • Documents
  • SigmaDSP YouTube Channel - Dave Thib
  • +AD193x: FAQ
  • +ADAU1401AEBZ: FAQ
  • +ADAU144x: FAQ
  • +ADAU1452: FAQ
  • +ADAU145x: FAQ
  • +ADAU1701: FAQ
  • +ADAU1701MINIZ- FAQ
  • +ADAU1761: FAQ
  • +ADAU1772: FAQ
  • +ADI: FAQ
  • +AN-951: FAQ
  • +bitwise logic: FAQ
  • +Compressor Table Format: FAQ
  • +Creating a simple balance crossfade control: FAQ
  • +Creating constant-dB envelope decay using an existing linear decay algorithm: FAQ
  • +Crossover with more than 3 bands: FAQ
  • +E2PROM: FAQ
  • +EEPROM: FAQ
  • +EVAL DAU144XEBZ: FAQ
  • +EVAL-ADAU1781Z: FAQ
  • +Excluding Cells from the Exported System Files: FAQ
  • +GPIO button: FAQ
  • +GPIOs or Aux ADCs: FAQ
  • +How do I execute a software safeload write?: FAQ
  • +IIR coefficient filter: FAQ
  • +IIR filter: FAQ
  • +Peak Full Range Compressor: FAQ
  • +Preserving "Ear-candy": FAQ
  • +Push Button Volume: FAQ
  • +self-boot EEPROM image: FAQ
  • +Sigma300 Family Products: FAQ
  • -SigmaDSP: FAQ
    • Booting a SigmaDSP from a microcontroller with no C compiler
    • Calculating Filter Coefficients to Store in a Microcontroller
    • Can I program multiple SigmaDSPs in parallel using one USBi?
    • Can I use SigmaDSP to decode MP3/WAV/AAC?
    • Can I write C or assembly code for SigmaDSP in SigmaStudio?
    • Can SigmaDSP do frequency-domain processing like FFT or pitch shift?
    • Can we bundle SigmaStudio with our product design?
    • Creating a delay after startup
    • Developing custom algorithms and/or using 3rd party algorithms
    • How can I estimate MIPS/Memory resource on SigmaDSP?
    • How do I create the microcontroller code to interface to my SigmaDSP?
    • How do I start a timer after power-on, or when the input signal goes away?
    • How many instructions can be executed per sample in SigmaDSP?
    • Memory requirements for booting a SigmaDSP with a microcontroller
    • Monitoring average and instantaneous signal levels
    • Playing audio samples in SigmaDSP
    • SigmaDSP PCB Layout Best Practices
    • SigmaDSP Products and Evaluation Boards - ROHS and REACH Compliance
    • SigmaStudio 3.4 Released
    • Updating SigmaDSP Parameter with a Microcontroller
    • Using two SigmaDSP evaluation boards simultaneously with one USBi board
    • Welcome to the SIGMADSP Processors and SIGMASTUDIO Development tool community
    • What are the number formats for SigmaDSP?
    • What is the step size for audio delay in a SigmaDSP?
    • What types of capacitors are good to use in the analog audio signal path?
    • Where can I buy a SigmaDSP Evaluation Board or USBi (EVAL-ADUSB2EBZ)?
    • Which SigmaDSP ICs support selfbooting from an EEPROM?
    • Which SPI Mode is used by SigmaDSP Devices?
    • Why isn't a software/documentation CD included with my evaluation board?
  • +SigmaStudio: FAQ
  • +single precision VS double precision: FAQ
  • +Stimulus-Probe Capability and Limitations: FAQ
  • +Stopwatch to Count Successive Samples: FAQ
  • +Toolbox into the schematic tab: FAQ
  • +USB communications between the PC and SigmaDSP: FAQ
  • +Using Hierarchy Boards to create re-usable code: FAQ
  • New SigmaStudio 3.2.0 beta version available
  • SigmaStudio 3.3 Released
  • SigmaStudio 3.9.2 Beta Available for Download
  • SigmaStudio Rev 3.15.2 Bug Report for SPI EEPROM Write Speed

Using two SigmaDSP evaluation boards simultaneously with one USBi board

Using two SigmaDSP evaluation boards simultaneously with one USBi board by BrettG

In order to evaluate more than one SigmaDSP at a time without the need for creating special prototype hardware, the USBi can be modified to connect with more than one evaluation board. In this example, a single USBi connects to two evaluation boards: the ADAU1781 and ADAU1761.

First of all, the USBi needs to be modified to add an extra connector to its ribbon cable. The connector simply crimps onto the existing cable and requires no soldering at all - the only tool I used was a vice to make sure the connection was tight. The part number on Digikey is MKC10K-ND, and the description is SOCK CONN 10 CONT OPEN W/POL GLD. The connector should be added to the ribbon cable with the same orientation (and by extension, pinout) as the existing 10-pin connector.

The following picture shows the basic setup. An MP3 player is used as an audio source. It feeds analog audio into the ADAU1761. The audio passes through the ADAU1761's ADCs and SigmaDSP core and then is output on the serial port to the ADAU1781 board. The ADAU1781 takes the audio in through its serial port, through its SigmaDSP core, and then outputs it through the DAC to the headphones.

NOTE: Clicking on the pictures in this post will increase their size.

The ADAU1781 board is the clock master, running off of its on-bard oscillator. It sends a master clock, LRCLK, and BCLK over to the ADAU1761 board, and receives data back from the ADAU1761's serial port. The connections were made here with simple fly-wires. Because the signals are somewhat high frequency (12.288 MHz for MCLK), the wires should be kept as short as possible to maintain signal integrity.

This picture shows the corresponding connections for the flywires on the ADAU1761 side.

The ADAU1781 and ADAU1761 boards will have the same I2C address by default. This needs to be modified in order to let the USBi differentiate between the two devices. Simply moving a resitor on the bottom of the ADAU1781 board will accomplish this goal.

The jumper/switch settings of the ADAU1781 board are shown here.

The jumper/switch settings of the ADAU1761 board are shown here.

In SigmaStudio, the USBi should be set up to communicate with the ADAU1781 and ADAU1761 on separate addresses, corresponding with the addresses used on the evaluation boards.

My basic audio flow has audio in from the ADAU1761 ADCs and out as I2S, then in as I2S to the ADAU1781 and out to its DACs. Of course, processing can be added here in SigmaStudio as necessary.

A working example project file is attached.

1761AnalogIn-DigitalOut_1781DigitalIn-AnalogOut.dspproj
  • Share
  • History
  • More
  • Cancel
 
Related Content
  • Between ADAU1761 and ADAU1781, are there any difference in serial data port ?
    Paramecium
    I have question about serial data port.Plese let me cofirm below. Are there any difference in serial data port between the ADAU1761 and the ADAU1781 ? When we use the ADAU1761's I2S in slave mode,...
  • ADAU1761 I2S slave mode with non-synchronous MCLK
    JohnAmpetronic
    Hello All I have a quick question about the use of the ADAU1761 I2S port in slave mode. I have tried the following experiment using an ADAU1761 and ADAU1701 evaluation kits. I created a simple...
  • Substituting ADAU1761 for ADAU1781
    chuckwin
    Hello, We just received notice that the ADAU1781 is in its last-time-buy phase. We would like to substitute the ADAU1761 in its place. I know the footprint is identical, and I know the dsp resources...
 
Related Content
  • Between ADAU1761 and ADAU1781, are there any difference in serial data port ?
    Paramecium
    I have question about serial data port.Plese let me cofirm below. Are there any difference in serial data port between the ADAU1761 and the ADAU1781 ? When we use the ADAU1761's I2S in slave mode,...
  • ADAU1761 I2S slave mode with non-synchronous MCLK
    JohnAmpetronic
    Hello All I have a quick question about the use of the ADAU1761 I2S port in slave mode. I have tried the following experiment using an ADAU1761 and ADAU1701 evaluation kits. I created a simple...
  • Substituting ADAU1761 for ADAU1781
    chuckwin
    Hello, We just received notice that the ADAU1781 is in its last-time-buy phase. We would like to substitute the ADAU1761 in its place. I know the footprint is identical, and I know the dsp resources...