Post Go back to editing

Developing Sigma DSP Cluster

Hi sirs

First, I 'm searching for people that uses the Sigma DSP (I trying to use AD1940).

My first project is to develop a AD1940 cluster to perform and audio routing system (with some improved features).

The basic project concept is :

http://jeanfernandes.com/files/images/dspsigmaex.pdf

The idea is to put all of them on same board.

Some questions:

a) Is it possible to wire the Audio Input Codec (as master) on 6 DSP without glue logic ?

b) And about the Master Clock ? Usually I use a hibrid square wave clock up to 3 chips. What glue logic is really necessary to

this project ?

c) Is it possible to draw the board just using 2 layers ?

d) I need to put audio compressor on all inputs and I saw that the curve has 32 points, but I dont know how to map an HMI user interface

to control all points of this block. My boss suggest me annotate several curves and list them to user choose (its a simple manner but ....)

e) If I use the TDM channel (to simplify design) what the maximum sampling rate (I suppose that is 48 Khz).

f) I will develop the controller firmware using C (ARM7). Does anyone has an SDK to control the IC's 1940 and 1939 (using SPI) ?

Regards

Jean Fernandes

Using Eval Mini AD1940 Evb to test.

attachments.zip
Parents Reply Children
No Data