Post Go back to editing

Can we bundle SigmaStudio with our product design?

We are designing an audio system using a SigmaDSP as the processor. Can we provide SigmaStudio to our end customers as a tuning tool to interface to our product?

Parents
  • Hello,

    I stumbled upon this article which has text that seems to conflict with the information in this thread.  The article is circa 2002 and could be outdated

    http://www.analog.com/library/analogDialogue/archives/36-01/sigmaDSP/index.html


    --snippet of text from article --

    "While the SigmaDSP GUI is intended as a dedicated tool for the system designer, it could also be made available (in a modified version) to the enthusiastic end user. With this PC interface, a user can have total control via a notebook PC."

    -- end snippet

    So is it possible to modify SigmaDSP and provide it to end user ?  This would lower cost for a device that falls into the 'set and forget ' category, such as a trunk mounted dsp with eq, crossover, etc.

    tia

    rperkins

Reply
  • Hello,

    I stumbled upon this article which has text that seems to conflict with the information in this thread.  The article is circa 2002 and could be outdated

    http://www.analog.com/library/analogDialogue/archives/36-01/sigmaDSP/index.html


    --snippet of text from article --

    "While the SigmaDSP GUI is intended as a dedicated tool for the system designer, it could also be made available (in a modified version) to the enthusiastic end user. With this PC interface, a user can have total control via a notebook PC."

    -- end snippet

    So is it possible to modify SigmaDSP and provide it to end user ?  This would lower cost for a device that falls into the 'set and forget ' category, such as a trunk mounted dsp with eq, crossover, etc.

    tia

    rperkins

Children
No Data