Post Go back to editing

How do I change the sample rate of my SigmaStudio system?

Thread Summary

The user asked how to change the default 48 kHz sample rate in SigmaStudio projects. The solution involves setting the sample rate in the toolbar, confirming the change, and linking-compile-downloading the project. For hardware, the core frame rate register must be set according to the specific IC (e.g., AD194x, ADAU144x, ADAU170x/ADAU1401, ADAU176x). For the ADSP-SC589_EZ evaluation board, the sample rate in SigmaStudio is for programming purposes, and the actual sample rate must be set via the DSP registers and clock configurations.
AI Generated Content
Parents Reply Children
  • Sorry, but I have the same question but now for my ADSP-SC589_EZ evaluation board, which is not included here.

    Are there any updated instructions on this issue?

    BN

  • Hello bnilsson,

    I would post this question on the SHARC section of this forum. 

    SigmaStudio will work the same way for the SHARC DSPs, the sample rate at the top of the window is only for SigmaStudio to properly program code that needs to know what the sample rate is. It is up to you to be certain that the registers in the DSP are properly set and the clocks going to the part are correct to obtain the desired sample rate inside the DSP. SigmaStudio does not know what rate the DSP is actually running at. 

    Dave T

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.