Post Go back to editing

Clock reset - EVAL-ADAU1701MNIB7 Sigma Studio

Hello,

I have a problem, as you can see from our attached files, i am using a button to control a clock cycle which in turns selects filter 0 to filter 3.

However, there is an issue whenever i link the program to the dsp board, it will randomly start at different filter selection which is not what we want.

Can i know how to reset the clock or how could I set the filter selection to be filter 0 whenever dsp loads ?

Thanks and Regards.

Parents
  • Hello JeradL,

    We are still unable to find the value edit option for interface read block with the new download as advised.

    While we are at it, can we know if this dsp board is able to read binary data sent from PC ?

    We would like to control the peaking filters, attenuation via binary input from the PC instead of the current configuration of using buttons.

    Thanks and regards.

    Edit : Are there any more IOs that we can use from this DSP board ? MP4 - MP6 are not listed on the PDF help file or so i thought.  Are we able to use it somehow ? We intend to wire wrap a RS 485 pin directly to the various usable IOs to control filter and volume selection

Reply
  • Hello JeradL,

    We are still unable to find the value edit option for interface read block with the new download as advised.

    While we are at it, can we know if this dsp board is able to read binary data sent from PC ?

    We would like to control the peaking filters, attenuation via binary input from the PC instead of the current configuration of using buttons.

    Thanks and regards.

    Edit : Are there any more IOs that we can use from this DSP board ? MP4 - MP6 are not listed on the PDF help file or so i thought.  Are we able to use it somehow ? We intend to wire wrap a RS 485 pin directly to the various usable IOs to control filter and volume selection

Children
No Data