Is there a way to use I2S or TDM to connect two sigmadsp adau1701's, One running 192khz sample rate and the other running 96khz sample rate.
ADAU1701
Production
The ADAU1701 is a complete single-chip audio system with a 28-/56-bit audio DSP, ADCs, DACs, and microcontroller-like control interfaces. Signal processing...
Datasheet
ADAU1701 on Analog.com
Is there a way to use I2S or TDM to connect two sigmadsp adau1701's, One running 192khz sample rate and the other running 96khz sample rate.
On the ADAU1701, the serial port rate should be running at the same rate as the SigmaDSP core. In order to connect two devices running at different sampling rates, you would need to use a sample rate converter (SRC) between the two serial ports. The AD1895 is a good choice for a stand-alone stereo SRC. The ADAU1442 and ADAU1445 SigmaDSPs also have integrated SRCs.
On the ADAU1701, the serial port rate should be running at the same rate as the SigmaDSP core. In order to connect two devices running at different sampling rates, you would need to use a sample rate converter (SRC) between the two serial ports. The AD1895 is a good choice for a stand-alone stereo SRC. The ADAU1442 and ADAU1445 SigmaDSPs also have integrated SRCs.