ADAU1361
Production
The ADAU1361 is a low power, stereo audio codec that supports stereo 48 kHz record and playback at 14 mW from a 1.8 V analog supply. The stereo audio ADCs...
Datasheet
ADAU1361 on Analog.com
Hi!
I am going to clock ADAU1361 CODEC core from its internal PLL using 12MHz external MCLK signal. I do the following:
1. Load PLL control register with 6 byte word described in the ADAU1361 Rev. C datasheet (Table 16, row 2) to lock at 45.1584MHz. This time I reset PLLEN bit to disable PLL according to the PLL initialization sequence presented in the datasheet (p. 25).
2. Load the same byte sequence to the PLL control register but set PLLEN bit to start locking.
3. Periodically poll PLL control register.
Each time I poll the PLL control register the Lock Bit equals zero i.e. PLL is not in lock. If I try to clock the core from MCLK signal directly it seems that all goes fine since I have acces to internal registers (can read their default values at least). What can be wrong with the PLL initialization?
Thank you in advance,
Vladimir.
Solved. I had my oscilloscope connected to MCLK line. All goes fine without the oscilloscope. It seems that some parasitics were introduced into MCLK line. Well, nice lesson.
Keep your clocks clean and sharp!
Vladimir.
Solved. I had my oscilloscope connected to MCLK line. All goes fine without the oscilloscope. It seems that some parasitics were introduced into MCLK line. Well, nice lesson.
Keep your clocks clean and sharp!
Vladimir.