Post Go back to editing

ADAV400 register dump using Sigmastudio

Hello,

I am working on a troublesome legacy design using ADAV400 audio DSP.

Can I get a register dump from the DSP without creating a project in Sigmastudio?

I hope to be able to boot from the existing host, then to switch I2C lines to USBi and try to read the registers of the DSP.

Does this idea make any sense?

Are there other ways to implement register dump without intervention from the existing host?

Thank you for your help!

Parents
  • I would be interested in hearing any discussion on this because this is the "easy" method to steal the code out of someone else's product. I am attempting to implement counter-measures for this sort of thing so no one can do it on mine. At least make the program disabled on startup so that some other external trigger non-SPI/I2C (MPx/ADC) enables audio output.

Reply
  • I would be interested in hearing any discussion on this because this is the "easy" method to steal the code out of someone else's product. I am attempting to implement counter-measures for this sort of thing so no one can do it on mine. At least make the program disabled on startup so that some other external trigger non-SPI/I2C (MPx/ADC) enables audio output.

Children
No Data