in case of crash

Does ADAU1701 have a watchdog? How do you recover from a crash?

Parents
  • Good layout practices are of key importance when dealing with a noisy system.

    • First of all, a solid ground plane is a necessity in order to  maintain signal integrity and minimize EMI radiation. I have seen many customers experience severe EMI issues when trying to design a PCB with no ground plane. If you have two  ground planes, I would recommend using stitching vias spead evenly  throughout the board in order to connect them.
    • Power supply high frequency decoupling capacitors should be placed  as close as possible to the respective power and ground pins, on the  same side of the board as the SigmaDSP IC. There should be no vias  between the pins and the decoupling caps. Please see the following  excerpt from the ADAU144x datasheet for more detail.

    • Typically, we use a single 100 nF capacitor for each power-ground  pin pair. However, if there is excessive high frequency noise in the  system, an additional 10 nF capacitor can be used in parallel. In that  case, the 10 nF capacitor should be closest, and the thermal connections  should be on the far side of the 100 nF capacitor.

    • 10 uF capacitors should be used for each named supply (DVDD, AVDD,  IOVDD, etc) in order to provide a current reservoir in case of sudden  current spikes.

    • The proximity of components to the IC is important. Here is my  suggested order which should be followed when placing components. The  top of the list begins with the components that should be placed closest  to the IC, and the bottom of the list has the components that can be  placed further away.
      • 10 nF high frequency decoupling capacitors
      • 100 nF high frequency decoupling capacitors
      • PLL filter components
      • Crystal
      • Current reservoir capacitors
Reply
  • Good layout practices are of key importance when dealing with a noisy system.

    • First of all, a solid ground plane is a necessity in order to  maintain signal integrity and minimize EMI radiation. I have seen many customers experience severe EMI issues when trying to design a PCB with no ground plane. If you have two  ground planes, I would recommend using stitching vias spead evenly  throughout the board in order to connect them.
    • Power supply high frequency decoupling capacitors should be placed  as close as possible to the respective power and ground pins, on the  same side of the board as the SigmaDSP IC. There should be no vias  between the pins and the decoupling caps. Please see the following  excerpt from the ADAU144x datasheet for more detail.

    • Typically, we use a single 100 nF capacitor for each power-ground  pin pair. However, if there is excessive high frequency noise in the  system, an additional 10 nF capacitor can be used in parallel. In that  case, the 10 nF capacitor should be closest, and the thermal connections  should be on the far side of the 100 nF capacitor.

    • 10 uF capacitors should be used for each named supply (DVDD, AVDD,  IOVDD, etc) in order to provide a current reservoir in case of sudden  current spikes.

    • The proximity of components to the IC is important. Here is my  suggested order which should be followed when placing components. The  top of the list begins with the components that should be placed closest  to the IC, and the bottom of the list has the components that can be  placed further away.
      • 10 nF high frequency decoupling capacitors
      • 100 nF high frequency decoupling capacitors
      • PLL filter components
      • Crystal
      • Current reservoir capacitors
Children
No Data