in case of crash

Does ADAU1701 have a watchdog? How do you recover from a crash?

Parents
  • There is no watchdog on the ADAU1701. If there is a crash, the device will need to be reset and initialized.

    SigmaStudio generates code that is 100% deterministic and does not contain any program counter jumps (conditionals, jumps, branches), and the "Return to Start" operation is hardware based, not software based, the chances of the program crashing are extremely small (limited to memory corruption).

    Message was edited by: BrettG. Changed "set" to "reset".

Reply
  • There is no watchdog on the ADAU1701. If there is a crash, the device will need to be reset and initialized.

    SigmaStudio generates code that is 100% deterministic and does not contain any program counter jumps (conditionals, jumps, branches), and the "Return to Start" operation is hardware based, not software based, the chances of the program crashing are extremely small (limited to memory corruption).

    Message was edited by: BrettG. Changed "set" to "reset".

Children
No Data