ADAU1701 - on-chip and External DAC problem

Hi All,

I have a problem with a new application with ADAU1701 DSP.

I would use both DSP DACs and an external CODEC, but after some tests I have the audio output on the ADAU1701 DACs or on the external CODEC DACs, but not both.

In my system I have an AK4620B CODEC as audio input ADCs and low noise stereo DACs, and I use also ADAU DAC2 and DAC3.

I have a 24.576MHz crystal and I used an internal fs=96kHz  (I used your faq instruction for PLL setting), the clock output is buffered and the DSP works as master of I2S comunication (MP4 and 5 connected with MP10 and 11 each).

I have test, with a simple audio path (attached TestInternalDac.jpg) that internal DAC works properly.

Only when I check the Master Mode checkbox in the Hardware Configuration windows the output signal disappeared.

Changing the outputs to I2S data I could see the audio signal on CODEC.

So...could I work with both outputs type or is not allowed?

Or have I make something wrong?

Thanks and best Regard.

attachments.zip