Hello,
I have to expand a digital-radio-transceiver for automotive applications by a DSP. The DSP has the task to equalize music by using various profils (e.g. rock, pop, flat, bass enhancement). The choice which profile will be used should be controlled by a microcontroller. Now I am looking for a suitable DSP. In summary the DSP has to fulfil following requirements:
-made for automotive applications
-I2C interface to communicate with the microcontroller
-I2S input and output
-max 5V supply voltage
-min. 2 MHz clock frequency at the I2S output
-EQ settings easy programmable
-EQ settings manageable by the microcontroller
I have found two DSPs which would be suitable but I do not know which one would be better for my application. I have found the AD1941 and ADAU1701.
I hope you can understand my request and help me
Regards,
Sebastian