ADAU1701
Production
The ADAU1701 is a complete single-chip audio system with a 28-/56-bit audio DSP, ADCs, DACs, and microcontroller-like control interfaces. Signal processing...
Datasheet
ADAU1701 on Analog.com
Hi,
I'm just wondering how can I find out how much memory I really need for my finished project in the EEPROM.
We have a design where we switch from the 1702 to the 1701 that has more processing power.
Further we have an 8kB EEPROM in the design for self-booting the device that should not be changed for the 1701.
The data sheet says that normally an 8kB should be sufficient for the 1701 (for the 1702 it's not a problem).
1) Is it simply program memory x4 Bytes + parameter memory x5 Bytes (if I do not use any writeback / interface registers)?
2) Can the "E2Prom.Hex" file give me the correct size? E.g. my "E2Prom.Hex" has 1012 line x8 Bytes so I need 8096 bytes total? What if more that 8192 bytes would be needed, will the "E2Prom.Hex" then have more than 1024 lines? Would there be an error message when I try to write such a project to the EEPROM?
Thanks
Christian
Yes, that's correct. Unfortunately, the ADAU1701 has no "jump to start" instruction, so the program must be filled with valid op-codes in order for it to operate. This necessitates 5120 bytes of program memory, regardless of the program size.
This problem was fixed in later SigmaDSPs like the ADAU1442 and ADAU1761, which have "jump to start" instructions.
Yes, that's correct. Unfortunately, the ADAU1701 has no "jump to start" instruction, so the program must be filled with valid op-codes in order for it to operate. This necessitates 5120 bytes of program memory, regardless of the program size.
This problem was fixed in later SigmaDSPs like the ADAU1442 and ADAU1761, which have "jump to start" instructions.