Post Go back to editing

Interfacing ADAU1761 x2

Hello,

I've been working with a pair of 1761 eval boards and have run into a mysterious clock sync problem. Every ~4 seconds I have a short amplitude reduction in the output signal. I'm hearing this as a very brief drop out or click in my headphones. Perhaps I've missed a register setting. The audio streams are otherwise working/sounding fine and I'm running them through a pair of the ADI beamforming algorithms.

Setup:

Passing a digital signal from the slave board to clock master. I've tried Left/Right Justified and TDM modes, following the configuration parameters from pg 42-43 in the ADAU1761 datasheet.

I've taken a look at this tutorial: http://ez.analog.com/message/5675#5675

Jumper configuration for my setup is consistent for clock sync and passing ADC to DAC pins. I've not had any luck setting MCLK to the I2S setting, both boards are set to OSC.

Any ideas?

Best,

John

Parents
  • Hi John,

    Running MCLK between two boards in that manner is a tricky thing. Did you run only the one wire, from the switch side of R47 on the MCLK source board, to the EXT_MCLK pin on the slave board? And also, did you run at least one ground wire along with the MCLK line? It is very important to reference the two boards together, using GND connections right near the places where you are attaching leads for MCLK.

    Let us know if this helps!

    Regards,

    Coleman

Reply
  • Hi John,

    Running MCLK between two boards in that manner is a tricky thing. Did you run only the one wire, from the switch side of R47 on the MCLK source board, to the EXT_MCLK pin on the slave board? And also, did you run at least one ground wire along with the MCLK line? It is very important to reference the two boards together, using GND connections right near the places where you are attaching leads for MCLK.

    Let us know if this helps!

    Regards,

    Coleman

Children
No Data