Post Go back to editing

Interfacing ADAU1761 x2

Hello,

I've been working with a pair of 1761 eval boards and have run into a mysterious clock sync problem. Every ~4 seconds I have a short amplitude reduction in the output signal. I'm hearing this as a very brief drop out or click in my headphones. Perhaps I've missed a register setting. The audio streams are otherwise working/sounding fine and I'm running them through a pair of the ADI beamforming algorithms.

Setup:

Passing a digital signal from the slave board to clock master. I've tried Left/Right Justified and TDM modes, following the configuration parameters from pg 42-43 in the ADAU1761 datasheet.

I've taken a look at this tutorial: http://ez.analog.com/message/5675#5675

Jumper configuration for my setup is consistent for clock sync and passing ADC to DAC pins. I've not had any luck setting MCLK to the I2S setting, both boards are set to OSC.

Any ideas?

Best,

John

Parents
  • Yes I have both boards externally powered and successfully deploy the programs. The clock signal pulled from R47 is not valid - we looked at it with a logic analyzer and its all over the place. I got a 1781 board setup today and it's driving the clock from MCLK0 to the 1761 MCLK input just fine.

Reply
  • Yes I have both boards externally powered and successfully deploy the programs. The clock signal pulled from R47 is not valid - we looked at it with a logic analyzer and its all over the place. I got a 1781 board setup today and it's driving the clock from MCLK0 to the 1761 MCLK input just fine.

Children
No Data