Post Go back to editing

ADAU1461 TDM problem

Hi. I have a custom prototype PCB with ADAU1461. Running in slave 8ch TDM

However I cannout get an output on the TDM SDO pin. Its always HIGH for bits 32-8 and LOW for 7-0 in the TDM slot.

See attached  DSP.JPG

my MCLK is 12.288mhz So I am using the PLL x4.

My Project even has a Fixed DC signal on one of the TDM slots  to see if the Problem is receiving or sending. and yet still no output.

Project attached.

Also attached is a DUMP of the Config registers unless I am missing something and surely I must be, They look ok to me.

I could really do with some help on this. I have run out of Ideas.

Thanks

Brett

attachments.zip
Parents
  • Hi Brett.

    thankfully I have an FPGA between the TDM master and the ADAU1461 SO I will have to Re format the data there. As the rest of my systen needs delay by 0  32 bit PCM data.

    I think there is a BUG is Sigma Studio  because all the TDM channel Numbers do not map as Per Fig 62 in the datasheet. Instead of Slots 0-7 being DIG0-7 in SS It appears to be DIG0 is Slot 0 (ie first ) and DIG1 is Slot 4

    If you simply create a tone signal source and map it to DIG1 output you will see what I mean.

    Thanks

Reply
  • Hi Brett.

    thankfully I have an FPGA between the TDM master and the ADAU1461 SO I will have to Re format the data there. As the rest of my systen needs delay by 0  32 bit PCM data.

    I think there is a BUG is Sigma Studio  because all the TDM channel Numbers do not map as Per Fig 62 in the datasheet. Instead of Slots 0-7 being DIG0-7 in SS It appears to be DIG0 is Slot 0 (ie first ) and DIG1 is Slot 4

    If you simply create a tone signal source and map it to DIG1 output you will see what I mean.

    Thanks

Children
No Data