Post Go back to editing

ADAU1461 TDM problem

Hi. I have a custom prototype PCB with ADAU1461. Running in slave 8ch TDM

However I cannout get an output on the TDM SDO pin. Its always HIGH for bits 32-8 and LOW for 7-0 in the TDM slot.

See attached  DSP.JPG

my MCLK is 12.288mhz So I am using the PLL x4.

My Project even has a Fixed DC signal on one of the TDM slots  to see if the Problem is receiving or sending. and yet still no output.

Project attached.

Also attached is a DUMP of the Config registers unless I am missing something and surely I must be, They look ok to me.

I could really do with some help on this. I have run out of Ideas.

Thanks

Brett

attachments.zip
Parents
  • Hi Brett.

    If I set the Delay to 0, All that happens is the Entire SDO bit stream shifts One Bit to the Left. Still No MSB.

    in fact it is impossible to have an MSB in this format as it would be truncated off.

    The fact that the SDI and SDO Bit patterns MATCH in timing perfectly with "delay by one" is really ODD concidering what your saying that the format of my SDI data is "delay bit by 0".

    Can you advise if the PROGRAM DATA changes once its loaded into the DSP?

    If I read back this , Its does not apprear the same as what I put in. All the Configuration data is though.

    Thanks

Reply
  • Hi Brett.

    If I set the Delay to 0, All that happens is the Entire SDO bit stream shifts One Bit to the Left. Still No MSB.

    in fact it is impossible to have an MSB in this format as it would be truncated off.

    The fact that the SDI and SDO Bit patterns MATCH in timing perfectly with "delay by one" is really ODD concidering what your saying that the format of my SDI data is "delay bit by 0".

    Can you advise if the PROGRAM DATA changes once its loaded into the DSP?

    If I read back this , Its does not apprear the same as what I put in. All the Configuration data is though.

    Thanks

Children
No Data