Post Go back to editing

ADAU1461 TDM problem

Hi. I have a custom prototype PCB with ADAU1461. Running in slave 8ch TDM

However I cannout get an output on the TDM SDO pin. Its always HIGH for bits 32-8 and LOW for 7-0 in the TDM slot.

See attached  DSP.JPG

my MCLK is 12.288mhz So I am using the PLL x4.

My Project even has a Fixed DC signal on one of the TDM slots  to see if the Problem is receiving or sending. and yet still no output.

Project attached.

Also attached is a DUMP of the Config registers unless I am missing something and surely I must be, They look ok to me.

I could really do with some help on this. I have run out of Ideas.

Thanks

Brett

attachments.zip
Parents
  • Well I finall got the DSP to output some signal.

    It turns Out the CHIP was defective all this time.

    I repalced it and YAY some output signal..

    BUT I do have one last question

    It appears the DSP is Not passing the First Bit.

    My Project has Nothing But ALL TDM inputs routed to ALL TDM Outputs in the DSP Schematic.

    See the Attached Screen Grab of the Logic Analyser

    Details

    MCLK  12.288M

    8ch TDM

    PLL at 4x

    SigmaStudio is set to

    TDM8 Slave 50%

    LRCK Falling

    BLCK Falling

    BitCLK cycles 256 per frame

    Data Delay LREdge =1

    REG 0x4015  = 0x04

    REG 0x4016 = 0x80

    is this correct for my incomming TDM Data?

    Thanks

Reply
  • Well I finall got the DSP to output some signal.

    It turns Out the CHIP was defective all this time.

    I repalced it and YAY some output signal..

    BUT I do have one last question

    It appears the DSP is Not passing the First Bit.

    My Project has Nothing But ALL TDM inputs routed to ALL TDM Outputs in the DSP Schematic.

    See the Attached Screen Grab of the Logic Analyser

    Details

    MCLK  12.288M

    8ch TDM

    PLL at 4x

    SigmaStudio is set to

    TDM8 Slave 50%

    LRCK Falling

    BLCK Falling

    BitCLK cycles 256 per frame

    Data Delay LREdge =1

    REG 0x4015  = 0x04

    REG 0x4016 = 0x80

    is this correct for my incomming TDM Data?

    Thanks

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.