Post Go back to editing

ADAU1442 with Two ADAU1701

Hello,

 

I am making a prototype for which my requirement is as given below:

 

1. SPDIF Input (1)

 

2. SPDIF Output (1)

 

3. Analog Input (at least 1 stereo channel)

 

4. Analog Output (at least 3 stereo channels)

 

For the above requirement, I think the least complex (cost-wise, component count wise) way is to use ADAU1442 with two ADAU1701/02.

 

Kindly guide me on my design thoughts below:

 

1. Use only one 12.288MHz crystal connected to ADAU1442 and use its MCLKO to drive the ADAU1701/2.

 

2. Use all three chips in selfboot  mode with their own EEPROMS. The contents of the two ADAU1701/2 may or may not be the same.

 

3. Set ADAU1442 address to 00 with its EEPROM address lines also set to 000

 

4. Set ADAU1701/2 to two different addresses 00, 01, 10 or 11 by using ADDR0 and ADDR1 lines. Say, 00 and 01.

 

5. Route the 2 x ADAU1701/2 ADC inputs to ADAU1442 for processing effectively using it only as a 2In, 4Out CODEC.

 

6. Route all the processed channels to the DACs of ADAU1701/2, effectively using it as a audio processor with SPDIF IN/OUT and SERIAL IN/OUT.

 


My doubts are as below:

 

1. For the ADAU1442:
  a. What should be the PLL0, PLL1 and PLL2 lines be set to?
  b. What should the CLKMODE0 and CLKMODE1 lines be set to?
  c. Will ADAU1446 also suffice in my case?

 

2. For the two ADAU1701/2:
  a. What should be the PLL0 and PLL1 lines be set to?
  b. What should be the EEPROM address lines be set to? I do not want to overwrite the SigmaStudio programmer EEPROM.

 


Any thoughts suggestions or corrections will be of much help to me.
DO let me know if you need any further details for better clarity.

 

Thanks in advance!

 

KKSL

Parents
  • Hello John,

    Thank-you for your early reply.

    I did consider the ADAU1451 and the AD1938 CODEC.

    The ADAU1451 is a new part and the algorithm libraries are not completely available/ported yet. If AD updates the SigmaStudio libraries soon, the AD145x can make its way in. I am designing from scratch and the schematics will not freeze in another 10 days.

    The AD1938 CODEC is nice, but it is costly. Moreover, it needs at least 8 low noise dual op-amps and the associated precision components for the ADC and DAC filters further adding to the cost and the real estate.

    Spec-wise, the AD1938 will measure better. However, sonically, will it be better?

    One elegant option is ADAV4601 which will need SPDIF Transceiver like WM8805, but it only gives me one stereo analog input.

    This one requires some additional micro controller based development, but it will only be a one time effort. If the requirement of two stereo analog inputs relaxes, this option could surge ahead.

Reply
  • Hello John,

    Thank-you for your early reply.

    I did consider the ADAU1451 and the AD1938 CODEC.

    The ADAU1451 is a new part and the algorithm libraries are not completely available/ported yet. If AD updates the SigmaStudio libraries soon, the AD145x can make its way in. I am designing from scratch and the schematics will not freeze in another 10 days.

    The AD1938 CODEC is nice, but it is costly. Moreover, it needs at least 8 low noise dual op-amps and the associated precision components for the ADC and DAC filters further adding to the cost and the real estate.

    Spec-wise, the AD1938 will measure better. However, sonically, will it be better?

    One elegant option is ADAV4601 which will need SPDIF Transceiver like WM8805, but it only gives me one stereo analog input.

    This one requires some additional micro controller based development, but it will only be a one time effort. If the requirement of two stereo analog inputs relaxes, this option could surge ahead.

Children
No Data