Post Go back to editing

ADAU1442 and linux network stack (TCPADAU1442)

Hello,

 

we are using the ADAU1442 in an embedded system and want to control the chip / unit via TCP and Sigmastudio using a TCP communication protocol. We are also using the ADAU1452 and want to do the same, see my other threads.

now i'm willing to test the "networked connection" thanx to the Network utility:

http://wiki.analog.com/resources/tools-software/linux-software/sigmatcp

anyway i've seen the TCP module in the communication tree of my sigmastudio 3.12 build1 rev.1422, has only three TCP modules for ADAU1761 ADAU1421 and 1940.

is there a more recent module for ADAU1442? Is this in the pipeline? Please contact me directly.

Best Regards and thank you,

Christian

Parents Reply Children
No Data