Post Go back to editing

Sync SPDIF Tx rate to SPDIF Rx rate

Hi,

I am planning a new product to use a SigmaDSP, the majority of the input/output will be analog (8 channel TDM converters). I will also use the SPDIF input as an extra stereo channel and I want to use the SPDIF output as a secondary output.

I can't run the core from the SPDIF input rate as it might not always be active, I will therefore present the SPDIF Rx to the core through an ASRC.

Now my problem, I want the SPDIF Tx active all the time but I want it to run in sync with the SPDIF Rx if it is there so:

how do I setup the SigmaDSP to feed an ASRC from the core and it's output to the SPDIF Tx?

Can I set the ASRC output rate to come from the SPDIF Rx?

What might happen to the Tx rate when I remove the signal from the Rx?

 

Thanks for any thoughts

PhilipJ

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.