Hi,
I am planning a new product to use a SigmaDSP, the majority of the input/output will be analog (8 channel TDM converters). I will also use the SPDIF input as an extra stereo channel and I want to use the SPDIF output as a secondary output.
I can't run the core from the SPDIF input rate as it might not always be active, I will therefore present the SPDIF Rx to the core through an ASRC.
Now my problem, I want the SPDIF Tx active all the time but I want it to run in sync with the SPDIF Rx if it is there so:
how do I setup the SigmaDSP to feed an ASRC from the core and it's output to the SPDIF Tx?
Can I set the ASRC output rate to come from the SPDIF Rx?
What might happen to the Tx rate when I remove the signal from the Rx?
Thanks for any thoughts
PhilipJ