ADAU1761
Production
The ADAU1761 is a low power, stereo audio codec with integrated digital audio processing that supports stereo 48 kHz record and playback at 14 mW from...
Datasheet
ADAU1761 on Analog.com
Hello all,
I am trying to give audio input through the microphone input ports (IN1 and IN2) of the EVAL-ADAU1X61EBZ board, but I am not able capture any signal from the output.
Anyone please tell me the settings/configuration needs to be done in order to give input through the microphone and to capture the output.
Thanks in advance,
Regards,
Vidhya
Hello,
Sorry it's still not working for you. I did not change any jumpers to get my board working as above, but perhaps your board's jumpers have been disturbed. Please check the following:
* Note: "Packaged" condenser mics (enclosed and ready to go on-stage) need "phantom power", usually a much higher DC voltage than the eval board provides. These cannot be directly connected to the eval board.
Does the eval board work with other inputs (such as a stereo input from a iPod or similar source to the IN 1 jack? It's a good idea to review the eval board's schematic diagram, comparing it to the ADAU1761 data sheet, to see how things should connect. For example, a single-ended mic needs to be connected "hot" to the ring (not the tip) of the stereo input jack IN1 or IN2.
Best regards,
Bob
Hello,
Sorry it's still not working for you. I did not change any jumpers to get my board working as above, but perhaps your board's jumpers have been disturbed. Please check the following:
* Note: "Packaged" condenser mics (enclosed and ready to go on-stage) need "phantom power", usually a much higher DC voltage than the eval board provides. These cannot be directly connected to the eval board.
Does the eval board work with other inputs (such as a stereo input from a iPod or similar source to the IN 1 jack? It's a good idea to review the eval board's schematic diagram, comparing it to the ADAU1761 data sheet, to see how things should connect. For example, a single-ended mic needs to be connected "hot" to the ring (not the tip) of the stereo input jack IN1 or IN2.
Best regards,
Bob