Post Go back to editing

ADAU1446 SPDIF recovered Clock as Master

Hi

Is it possible you use the recovered clock from the SPDIF receiver to be the clock source for the SDATA and DSP Core

My Project uses external Codec IC  as a slave that is connected to SDATA , and just one SPDIF I/O interface

So If I can Clock the Codec IC and The DSP from the Recovered SPDIF clock then I wont need SRC.

Is this Possible , I cannot see where to set the Clock domains to the SPDIF recovered clock.

Thanks

Brett

Parents
  • Hello Brett,

    I have not tried this myself yet so I might have a detail missing but give this a go.

    The DSP start pulse register is where you will tell it to get its clock rate from the SPDIF. See table 12 in the datasheet. It is Register 0xE220 and you will see setting 0b11011 is from the SPDIF.

    So the clocks to the CODEC you can simply set to use the DSP rate and I am pretty sure it will follow it.

    So give that a try and I think it should work.

    The only issue you may run into is that when you lose SPDIF you will lose all your clocks. So the CODEC will lose its clocks and you may end up with DC on the output when it stops seeing clocks. You could have some clicks or pops. Try it and let me know what happens.

    Dave T

Reply
  • Hello Brett,

    I have not tried this myself yet so I might have a detail missing but give this a go.

    The DSP start pulse register is where you will tell it to get its clock rate from the SPDIF. See table 12 in the datasheet. It is Register 0xE220 and you will see setting 0b11011 is from the SPDIF.

    So the clocks to the CODEC you can simply set to use the DSP rate and I am pretty sure it will follow it.

    So give that a try and I think it should work.

    The only issue you may run into is that when you lose SPDIF you will lose all your clocks. So the CODEC will lose its clocks and you may end up with DC on the output when it stops seeing clocks. You could have some clicks or pops. Try it and let me know what happens.

    Dave T

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.