Post Go back to editing

Queries related to ADAV4601

I am working on a custom ADAV4601 board and USBi.

I am powering up the IC using I2C script window.

I am able to successfully power-up the IC and load a custom flow.

1. Is there a Delay command that I can insert between the two 34 AAAA DDDD WRITEs?

e.g.

34 AAA1 DDD1

Delay 15ms

34 AAA2 DDD2

I have realized that the 15ms delay after powering up the PLL is very critical.

For now I just delay the WRITEs manually.

2. Is the ADI Surround block buggy?

There is no dialogue anchoring in the center channel and the surround channels have dialogue leakage.

If yes, can AD fix it? This block is the reason for me to look beyond the ADAU1701.

3. Can I have access to the application layer software mentioned in the ADAV46xx system document, which b.t.w. is very well written?

Thanks in advance and regards,

  • Alright, I understand that there is hardly any support available for ADAV4601 and hence queries 1 and 3 would be difficult to look into.

    However, can anyone using the ADAU144x or the ADAU145x comment on the performance of the ADI Surround block?

    1. Is the block capable of producing/ decoding stereo to 'dialogue-leakage-free' surround?

    2. If yes, are the surround channels stereo or mono?

    3. Does the block procuce/ decode the dialogue (mono content in stereo input) predominantly from the center channel?

    4. Do the Left and the Right channels produce the necessary separation, while retaining the dialogues anchored to the Center channel?

    In short: Can we look to ADI surround block as a poor man's Dolby Pro-Logic II block?

    Thanks!!

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.