Post Go back to editing

ADAU1772 analog input protection

I use the ADAU 1772 in a non-portable circuitry that is supplied with regular +\- 12V supplies.

The ADAU1772  itself is supplied with 3.3V.

This means that the op-amp that precedes the ADAU1772 analog inputs can deliver much more voltage than the analog inputs can handle (Vcc+0.3 - GND-0.3 V).

Now my question is whether the inputs are protected by diodes such that I can prevent overload by a series resistor, like with many C-Mos devices. And if so, what current can these input protecting diodes handle?

thanks, Rob

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.