ADAU1701
Production
The ADAU1701 is a complete single-chip audio system with a 28-/56-bit audio DSP, ADCs, DACs, and microcontroller-like control interfaces. Signal processing...
Datasheet
ADAU1701 on Analog.com
Hey All,
I was trying to configure an ADAU1701 connected to a raspberry pi (over an i2c bus, running Raspbian) using SigmaTcp. Unfortunately, I was unable to do that in the first attempt. I analyzed the TCPIP packages sent by SigmaStudio using wireshark and I noticed that the header was different from the one that SigmaTcp was waiting. Sigma tcp waits for a 8 bytes header, with length in the bytes 4 and 5, and addr in the bytes 6 and 7. SigmaStudio sends a 10 bytes header with length in the bytes 6 and 7, and addr in the bytes 8 and 9. After some changes in function handle_connection on sigma-tcp.c, I was able to control the chip over a TCP/IP connection.
Is there a different version of sigma tcp to be used with ADAU1701? I searched in this forum and couldn't find anyone with the same problem, so I decided to post this.
Thanks!
Lucas@
I don't understand why Analog doesn't respond to that either.
I already know the link you mentioned, but this package order only applies to the ADAU 144x and 145x - not to the ADAU1701.
I already tested it, but it didn't work out.
I don't understand why Analog doesn't respond to that either.
I already know the link you mentioned, but this package order only applies to the ADAU 144x and 145x - not to the ADAU1701.
I already tested it, but it didn't work out.