Hi,
I have a problem when load the EQ parameters on ADAU1451.
I build a 28 band EQ. T
The first parameter address is: 0x002B //DM0
The second parameter address is: 0x600E//DM1
The third parameter address is: 0x0030
The fourth parameter address is: 0x6013
Interleaving addresses.....and goes on, until 28 EQ.
When i load parameters into addresses 0x002B, 0x0030, ....,0x0071 there is no problem. At DM0.
But when i try to load into 0x600E, ,0x6013,..., 0x604A is a problem, the audio begins click and distortion comes.At DM1.
The parameters are the same and load in direct write during inicialization, i don´t know why. Am I missing any thing?