ADAU1701
Production
The ADAU1701 is a complete single-chip audio system with a 28-/56-bit audio DSP, ADCs, DACs, and microcontroller-like control interfaces. Signal processing...
Datasheet
ADAU1701 on Analog.com
Hi
My customer is trying to initiate an i2c read from adau1701.
Addr0==Addr1=0 => Write addr = 0x68, Read addr = 0x69.
Sequence looks like he indeed sends 0x69, however adaqu1701 doesn't send an ack (pulls SDA low on 9th clock)
Attached are read sequence & schematics.
Similar write sequence (sending 0x68) produces the required ack.
Please advise
BR,
Alon
Hello Alon,
Yes, it needs a write before a read. That is the way the state machine is setup. You cannot just send a start with the bit set to read. It must be a repeated start after the write setting the read address.
Dave T
Hello Alon,
Yes, it needs a write before a read. That is the way the state machine is setup. You cannot just send a start with the bit set to read. It must be a repeated start after the write setting the read address.
Dave T