Post Go back to editing

ADUA1462 Program and Data memory size

Hi,

Please let me confirm memory size of the ADAU1462.

On the ADI web page and data sheet ( rev.A ), we can find below. Is it correct values ?

http://www.analog.com/media/en/technical-documentation/data-sheets/ADAU1462-1466.pdf 

  Page 3 Table1. Product Selection Table
  ADAU1462 Data memory 48(KWords) Prgram Memory 16(Kwords)


But on the data sheet ( rev.A ), we can find different values.
The table 58 shows that ADAU1462's program memory size is 8 Kwords
It seems that the Figure 82 for the ADAU1466 illustrates the ADAU1462, but the program memory size is 8K words
It seems that the Figure 83 for the ADAU1462 illustrates the ADAU1466.

  Page 88 Table 58. ADAU1462 Memory Map
  Address Range         Length
  0xC000 to 0xCFFF      4096 words
  0xC000 to 0xCFFF      4096 words

  Page 89 Figure 82. ADAU1466 Slave Port Memory Map and the Mapping onto the SigmaDSP Core Memory
  Page 90 Figure 83. ADAU1462 Slave Port Memory Map and the Mapping onto the SigmaDSP Core Memory

On the other hands, on the Sigma Studio ver3.15.2 beta,
when putting the ADAU1462 in the project and build the schematic, we can see following messages.
The data program size is 40 Kwors.

###### IC 1 ######
ADAU145X Assembler, Analog Devices Inc.
Version: 3.15.2,1721  (built 6/29/2017)

##### Compile Started: Thursday, October 12, 2017 7:03:52 PM #####
##### Compile succeeded:  0 errors, 0 warnings #####

##### Summary #####
DM0 RAM used:       00024    (of 20480)
DM1 RAM used:       00013    (of 20480)
PM  RAM used(Data): 00000    (of 16384)
PM  RAM used(Inst): 00083    (of 16384) 71 instructions (32bit: 59  64bit: 12)
Total PM used:      00083    (of 16384)

Parents
  • Thank you for pointing out these important errors in the documentation. Table 3 is correct. The ADAU1462 has 16 kWords of program memory. Here is the corrected version of Table 58:

    This is the corrected version of Figure 89. Note that it is identical to Figure 26:

    This is the corrected version of Figure 90. Note that it is identical to Figure 27:

    Thank you for this errata report. A revised data sheet will be posted to the web site soon. Please let me know if you have any additional questions.

    Ken

Reply
  • Thank you for pointing out these important errors in the documentation. Table 3 is correct. The ADAU1462 has 16 kWords of program memory. Here is the corrected version of Table 58:

    This is the corrected version of Figure 89. Note that it is identical to Figure 26:

    This is the corrected version of Figure 90. Note that it is identical to Figure 27:

    Thank you for this errata report. A revised data sheet will be posted to the web site soon. Please let me know if you have any additional questions.

    Ken

Children
No Data