Post Go back to editing

Can ADAU1467 be used to build microphone array?

I want to build a mic array. Can I use ADAU1467 for that? Is it pre-programmed or graphically programmable?

Parents

  • Hello ,

    Sorry for the delayed response.

    Please note that up to four PDM microphones can be connected as audio inputs. Each pair of microphones can share a single data line; therefore, using four PDM microphones requires two GPIO pins. Any multipurpose pin can be used as a microphone data input, with up to two microphones connected to each pin. This configuration is set up using the corresponding MPx_MODE and DMIC_CTRLx registers.

    Please refer the DIGITAL PDM MICROPHONE INTERFACE (PageNo: 77 / 207) in the datasheet of ADAU146x.
    www.analog.com/.../ADAU1463-1467.pdf

    Regards,
    Lalitha.S

Reply

  • Hello ,

    Sorry for the delayed response.

    Please note that up to four PDM microphones can be connected as audio inputs. Each pair of microphones can share a single data line; therefore, using four PDM microphones requires two GPIO pins. Any multipurpose pin can be used as a microphone data input, with up to two microphones connected to each pin. This configuration is set up using the corresponding MPx_MODE and DMIC_CTRLx registers.

    Please refer the DIGITAL PDM MICROPHONE INTERFACE (PageNo: 77 / 207) in the datasheet of ADAU146x.
    www.analog.com/.../ADAU1463-1467.pdf

    Regards,
    Lalitha.S

Children
No Data