Post Go back to editing

Where to write in EEPROM "set multiple writeback" ?

Here the problem. I read in the ADAU1701 datasheet, that I have to set "Set multiple writeback" so that every time I change parameters, a writeback occurs... By default writeback is only enabled "one time" (normally used during power down). Could someone show me the position and the value of the byte I have to modify? In Sigmastudio Hardware configuration IC2, in the Display File, could someone tag the hex number I have to change to set multiple writeback? There's something other parameter to "enable" writeback in the EEPROM?

Thanks a lot,

Charlie.

Parents
  • Hi Dave, I'm really sorry for the impossibility to write a single byte and the programmer doesn't calculate the checksum. 

    Do you know if the checksum  is one byte or two bytes ? I could try to insert manually after having modified it accordingly. No one in Analog Device could help you in finding the location in EEPROM?

    No problem for waiting. 

    Thanks a lot,

    Charlie.

Reply
  • Hi Dave, I'm really sorry for the impossibility to write a single byte and the programmer doesn't calculate the checksum. 

    Do you know if the checksum  is one byte or two bytes ? I could try to insert manually after having modified it accordingly. No one in Analog Device could help you in finding the location in EEPROM?

    No problem for waiting. 

    Thanks a lot,

    Charlie.

Children
No Data