This is a battery powered microphone system consisting of 2 digital MEMS microphones, ADAU1788 for DSP, nPM1100 for power management, and nRF5340 for bluetooth transmission.
The requirements on the ADAU1788 are as follows:
- Receive two DMIC signals (rising edge and falling edge) on DMIC01 and DMIC_CLK0
- I2C interface with nRF5340
- Receive power from nPM1100 VOUTB pin (VDD on schematic)
- Process microphone signals with delay, subtraction, filtering, and EQ
- Output processed signal to nRF5340 via I2S
- Detect headphone connection via GPIO pin (MP3 on schematic)
- Unmute/output DAC headphone signal upon headphone connection
Design notes:
- The output signal is mono since the two DMIC signals are combined in processing.
- My headphone connection is based on Stereo Output in Figure 34. This reference shows the differential output pins on an ADAU connected to the single-ended headphone jack leads. However, since my signal is mono, T and R on the jack will need the same signal. Did I implement this correctly? Did I implement headphone jack detection in the recommended way?
- I have *PD connected to a GPIO on the nRF5340.

Any and all critique is welcome. I can provide additional schematic for other components if needed for review of this ADAU1788 implementation.
Thank you!