I've been asked to reconfigure our dev board to 192KHz from 48KHz. So I decided to start with the eval board first.
I asked AI for some help with this but it gave most of the registers different names and just added to my confusion. In SigmaStudio the PGA/ADC tab in Hardware Configuration has a Sample Rate section for ADC0/1 and ADC2/3 for 192KHz or 96 KHz. Also in the Output/Serial Port tab there is a Serial Port FS set to 48KHz or most any other desired rate. I'm left confused why 48KHz isn't an option in the PGA/ADC tab but is in the Serial Port FS tab, and why there are two areas to set... AI didn't cover using these; instead it ask for bit/byte setting with the Read/Write tab app.
Barry