Post Go back to editing

Indirect Parameter Access Table

Category: Software
Product Number: ADAU1467
Software Version: 4.7

Hi, Having issues with the IPAT.  I have enabled the proper options, built a table, did the update, recompiled and then stored to EEPROM.  For some reason, I cannot access the IPAT addresses, just the original register values in the schematic.  I have read through the other discussions on this and the IPAT documentation, but Squelch PL Decode 020726 IPAT A.dspprojdon't seem to see where I am missing the mark.  Can you take a look and see if something obvious with my table config?  Thanks!  Elsa.

Parents
  • AH, that might be the issue, if I am understanding you, correctly.   I have a program in my PI that allows me to write and read any register over my SPI connection.  I know I have the correct syntax as I can easily read and write to the schematic register values, so it looks like I need to change the syntax to do the dual read requests.  I did not think of using the register capture in SS to try the indirect parameter value, so I will study the syntax, there and make correction to the syntax.  I will do some further testing and let you know.  Thanks, Dave!

Reply
  • AH, that might be the issue, if I am understanding you, correctly.   I have a program in my PI that allows me to write and read any register over my SPI connection.  I know I have the correct syntax as I can easily read and write to the schematic register values, so it looks like I need to change the syntax to do the dual read requests.  I did not think of using the register capture in SS to try the indirect parameter value, so I will study the syntax, there and make correction to the syntax.  I will do some further testing and let you know.  Thanks, Dave!

Children
No Data