Post Go back to editing

On/OFF Sigma Studio+

Category: Software
Product Number: EVAL-ADAU1467Z
Software Version: 2.3.0 Update 4

I migrated to SS+ and am having a bit of a snag with the ON/OFF. I was using this as an easy register write to toggle an AND gate with a logic 1 in SS, but it does not seem to be functioning the same way in SS+ .  I noticed it is 32.0 format.  Is there some configuration to set this to 8.24 or is that needed in this application?  I am using a DC source to read/write for now, but would like to simplify.  

Thanks!

Parents
  • Hello ElsaDog,

    Yes, for some strange reason the programmers decided to only have one switch!! fortunately, it is fairly easy to translate this since this DSP has a hardware shift register accelerator so it does not take many DSP cycles. 

    Here is how you do it. You can see I added some Readbacks to show the change. Note the format of the ReadBacks. 

    Thanks!

    Dave T

Reply
  • Hello ElsaDog,

    Yes, for some strange reason the programmers decided to only have one switch!! fortunately, it is fairly easy to translate this since this DSP has a hardware shift register accelerator so it does not take many DSP cycles. 

    Here is how you do it. You can see I added some Readbacks to show the change. Note the format of the ReadBacks. 

    Thanks!

    Dave T

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.