Post Go back to editing

Help designing a variable HPF/LPF with adjustable resonance?

Category: Hardware
Product Number: ADAU1701

I am wondering if the 1701 is capable of running a high/low pass audio filter whose frequency and Q (resonance) I can control with pots.

I am a DJ, and am hoping to cook up a device that works similar to the Menura MDFX HP/LP so I can apply adjustable high and low pass filtering effects to my music. My mixer doesn't have a built-in filter stage like many higher end units and the Menura is cost prohibitive. I want to make a small standalone unit that I can put in the signal chain via the RCAs on a dspb-k board, to give me filter control.

Goals: 1 knob each for high and low pass adjustment. Full frequency at the extreme left of the pot rotation, with cutoff increasing through a specified frequency range with rotation to the right. Or alternatively one single knob with full frequency in the middle of the rotation, high cut to the left and low cut to the right. The third knob would adjust Q for resonance effect. The last pot would be made a switch to engage and disengage the effect. 18dB/octave slope.

Is the 1701 capable of this, and if so can anyone help me with the programming. I have only done simple, fixed 2.1 crossover projects up to now.

Thanks! 

Parents Reply
  • Hello Filterproject,

    You are not 100% correct about the limit of 63. If you set the input format to fractional then 63 is the limit because it is looking for a 5.23 number but if you set it for Integer input then it takes a 28.0 number so the table could be huge!! You will run into memory issues eventually. 

    Then, your comment about it being choppy does not take into account that we have a slew for the filter. When you change between two filters it will slew the filter coefficients from the old filter setting to the new one. This will help it not be choppy but also keeps the filter stable. 

    The ADAU1701 is one of our early SigmaDSP but is still a great solution and cost effective. If you need higher performance then jump up to the ADAU1452 and an external codec. 

    I am planning on making some videos about how to use lookup tables. It is high on my "ToDo" list for this spring!

    Dave T

Children
  • Hi Dave, 

    Thanks for the reply. I guess I'm in well over my technical understanding level. The reason I am trying to work with the 1701 is because I just happen to have one on hand that I was previously using for a basic 2.1 audio project and hoped to re-purpose.

    My inspiration is the filter on this and similar mixers - starting at 9:57 

    youtu.be/RS0wm4n_C7M

    In retrospect I'm not even sure that I need variable Q, especially if that's going to take valuable processing headroom needed for the frequency table. At the end of the day I am just looking for is a sweepable filter (or filters) with a 250Hz starting low cut point and a 2.5 KHz starting high cut point on an 18db/oct slope, but I need it to have a smooth, organic sweep like that mixer. If the 1701 is capable of pulling that off then I'm all ears.