Post Go back to editing

Help designing a variable HPF/LPF with adjustable resonance?

Category: Hardware
Product Number: ADAU1701

I am wondering if the 1701 is capable of running a high/low pass audio filter whose frequency and Q (resonance) I can control with pots.

I am a DJ, and am hoping to cook up a device that works similar to the Menura MDFX HP/LP so I can apply adjustable high and low pass filtering effects to my music. My mixer doesn't have a built-in filter stage like many higher end units and the Menura is cost prohibitive. I want to make a small standalone unit that I can put in the signal chain via the RCAs on a dspb-k board, to give me filter control.

Goals: 1 knob each for high and low pass adjustment. Full frequency at the extreme left of the pot rotation, with cutoff increasing through a specified frequency range with rotation to the right. Or alternatively one single knob with full frequency in the middle of the rotation, high cut to the left and low cut to the right. The third knob would adjust Q for resonance effect. The last pot would be made a switch to engage and disengage the effect. 18dB/octave slope.

Is the 1701 capable of this, and if so can anyone help me with the programming. I have only done simple, fixed 2.1 crossover projects up to now.

Thanks! 

Parents Reply Children
No Data