Post Go back to editing

source selection using adc potentiometer

Thread Summary

The user asked if it's possible to select one of several inputs using an analog potentiometer connected to the auxiliary ADC on the ADAU1701. The support engineer provided an example project for an index-selectable filter, which can be adapted for input MUX selection. The value from the auxiliary ADC is in 5.23 format (0...1). The user inquired about the circuit's resistance to transients and suggested implementing hysteresis.
AI Generated Content
Category: Software

Hi,
Is there a way to select one of several inputs using an analog potentiometer connected to the auxiliary ADC on the adau1701?

Just like in the attached image.

Thanks for your reply. Regards.

Parents Reply Children
No Data