Hello,
I have a problem with the ADAU1777 DSP mounted on a PCB. I am unable to write to certain registers, namely DAC0 mute and DAC0 enabled. I have seen that this is because the DSP's internal PLL must be locked in order to have write access to certain registers. However, I am unable to lock this PLL. I am using a frequency of 20MHz on the MCLKin input. I am interfacing the DSP with the I2C link, which seems to be working because I can write to certain registers with Sigmastudio 4.7. I am using IOVDD 3.3V, and my clock signal is 1.68V, which may not be sufficient. I tried injecting a clock with an amplitude of around 2.5V, but the software tells me “communication failed” during upload, as if the clock voltage were too high. Do you have any ideas on how to lock the PLL so that I can program the registers?
Below is a screenshot of my interface. You can clearly see that register 0x0006 has the value 0x00, meaning it is unlocked.
I am also including the project with the sigma studio file that I use.
Thank you.
Best regards,