My ADAU1452 takes a TDM8 signal in SDATA_IN0. I then want to output this TDM8 signal to SDATA_OUT2.
I have the following configuration in SigmaStudio:


This is my schematic (very simple, I just want to get it to work):

When I run this project, I do not see the BCLK_OUT2 running or the LRCLK_OUT2 running, even though I have set SDATA_OUT2 clocks correctly.
I previously had this working with a ADAU1401. We now need to use the ADAU1452. Here is my ADAU1401 setup:

Apologies if this question seems ignorant. I'm sure the answer is simple, I just can't seem to figure it out!
If I change the PLL CLK SRC to use the MCLK directly, I do get a BCLK and LRCLK, however not the right frequencies, and in the data sheet it explicitly says 'In most use cases, do not use the direct XTALIN/MCLK input option because the range of allowable frequencies on the XTALIN/MCLK pin is is an upper limit that is significantly lower in frequency than the nominal system clock frequency.'
Any help would be greatly appreciated.
Cheers,
Daz